2011-04-06 2:11 AM
MultiChannel(Scan) Continuous conversion mode of ADC sampling returns all 0s
2011-05-17 5:30 AM
I tried to verify if at least DMA transfer is happening.. I see that it is not...I have put following code and DMA_GetFlagStatus always remains RESET. So, the control does not come out of that.. Does that ring any bell?
/* Test on DMA1 channel1 transfer complete flag */
while(!DMA_GetFlagStatus(DMA1_FLAG_TC1));
/* Clear DMA1 channel1 transfer complete flag */
DMA_ClearFlag(DMA1_FLAG_TC1);
Thanks,
Sai
2011-05-17 5:30 AM
I tried to verify if at least DMA transfer is happening.. I see that it is not...I have put following code and DMA_GetFlagStatus always remains RESET. So, the control does not come out of that.. Does that ring any bell?
It helps to plug in the bell first. /* Enable DMA1 clock */ RCC_AHBPeriphClockCmd(RCC_AHBPeriph_DMA1, ENABLE);2011-05-17 5:30 AM
Thanks a lot Clive1... In deed that was the issue....
Now, I could gather values with little problem.. I am seeing some non-zero(up to a decimal value 18) value on the adjacent channel as well. I am using an array of 6 values to gather values from 6 channels as specified in my code.
Thanks,
Sai
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.