2020-08-07 5:38 AM
Hello, I am using L031K6 with its board
I am trying to sense multi- adc port. One is ADC 1 channel 3, other one is ADC1 channel 7
I open example code of ADC_DMA and overwrite it, for making my MCU sense these ADC channels, CH 3 & CH 7
but problem is, when I connect 3.3V to CH3 , CH7 is also increasing its ADC sense value , vice versa.
precisely, when I give 3.3v to ADC 1 CH 7, the CH3 adc value returns 4096 and it is correct because L031K6 ADC bits is 12bit. but the CH3 - which is not physically related - returns about 3000 ( check the screenshots, First one is default status, second is connecting to CH7 , When connecting to CH 3 then even number index array is 4096, others are about 3000 )
is it because these port are same ADC? or Do I set something wrong ?
thanks for reading.
below is my code:
//msp
void HAL_ADC_MspInit(ADC_HandleTypeDef *hadc)
{
GPIO_InitTypeDef GPIO_InitStruct;
static DMA_HandleTypeDef DmaHandle;
/*##-1- Enable peripherals and GPIO Clocks #################################*/
/* Enable GPIO clock ****************************************/
__HAL_RCC_GPIOA_CLK_ENABLE();
/* ADC1 Periph clock enable */
ADCx_CLK_ENABLE();
/* Enable DMA1 clock */
__HAL_RCC_DMA1_CLK_ENABLE();
/*##- 2- Configure peripheral GPIO #########################################*/
/* ADC Channel GPIO pin configuration */
GPIO_InitStruct.Pin = GPIO_PIN_3 | GPIO_PIN_7;
GPIO_InitStruct.Mode = GPIO_MODE_ANALOG;
GPIO_InitStruct.Pull = GPIO_NOPULL;
HAL_GPIO_Init(ADCx_CHANNEL_GPIO_PORT, &GPIO_InitStruct);
/*##- 3- Configure DMA #####################################################*/
/*********************** Configure DMA parameters ***************************/
DmaHandle.Instance = DMA1_Channel1;
DmaHandle.Init.Direction = DMA_PERIPH_TO_MEMORY;
DmaHandle.Init.PeriphInc = DMA_PINC_DISABLE;
DmaHandle.Init.MemInc = DMA_MINC_ENABLE;
DmaHandle.Init.PeriphDataAlignment = DMA_PDATAALIGN_HALFWORD;
DmaHandle.Init.MemDataAlignment = DMA_MDATAALIGN_HALFWORD;
DmaHandle.Init.Mode = DMA_CIRCULAR;
DmaHandle.Init.Priority = DMA_PRIORITY_MEDIUM;
DmaHandle.Init.Request = DMA_REQUEST_0;
/* Deinitialize & Initialize the DMA for new transfer */
HAL_DMA_DeInit(&DmaHandle);
HAL_DMA_Init(&DmaHandle);
/* Associate the DMA handle */
__HAL_LINKDMA(hadc, DMA_Handle, DmaHandle);
/* NVIC configuration for DMA Input data interrupt */
HAL_NVIC_SetPriority(DMA1_Channel1_IRQn, 1, 0);
HAL_NVIC_EnableIRQ(DMA1_Channel1_IRQn);
}
//main
/* ### - 1 - Initialize ADC peripheral #################################### */
AdcHandle.Instance = ADCx;
if (HAL_ADC_DeInit(&AdcHandle) != HAL_OK)
{
/* ADC de-initialization Error */
Error_Handler();
}
AdcHandle.Init.ClockPrescaler = ADC_CLOCK_SYNC_PCLK_DIV2; /* Synchronous clock mode, input ADC clock with prscaler 2 */
AdcHandle.Init.Resolution = ADC_RESOLUTION_12B; /* 12-bit resolution for converted data */
AdcHandle.Init.DataAlign = ADC_DATAALIGN_RIGHT; /* Right-alignment for converted data */
AdcHandle.Init.ScanConvMode = ADC_SCAN_DIRECTION_FORWARD; /* Sequencer disabled (ADC conversion on only 1 channel: channel set on rank 1) */
AdcHandle.Init.EOCSelection = ADC_EOC_SINGLE_CONV; /* EOC flag picked-up to indicate conversion end */
AdcHandle.Init.LowPowerAutoPowerOff = DISABLE;
AdcHandle.Init.LowPowerFrequencyMode = DISABLE;
AdcHandle.Init.LowPowerAutoWait = DISABLE; /* Auto-delayed conversion feature disabled */
AdcHandle.Init.ContinuousConvMode = ENABLE; /* Continuous mode enabled (automatic conversion restart after each conversion) */
AdcHandle.Init.DiscontinuousConvMode = DISABLE; /* Parameter discarded because sequencer is disabled */
AdcHandle.Init.ExternalTrigConv = ADC_SOFTWARE_START; /* Software start to trig the 1st conversion manually, without external event */
AdcHandle.Init.ExternalTrigConvEdge = ADC_EXTERNALTRIGCONVEDGE_NONE; /* Parameter discarded because software trigger chosen */
AdcHandle.Init.DMAContinuousRequests = ENABLE; /* ADC DMA continuous request to match with DMA circular mode */
AdcHandle.Init.Overrun = ADC_OVR_DATA_OVERWRITTEN; /* DR register is overwritten with the last conversion result in case of overrun */
AdcHandle.Init.OversamplingMode = DISABLE; /* No oversampling */
AdcHandle.Init.SamplingTime = ADC_SAMPLETIME_7CYCLES_5;
/* Initialize ADC peripheral according to the passed parameters */
if (HAL_ADC_Init(&AdcHandle) != HAL_OK)
{
Error_Handler();
}
/* ### - 2 - Start calibration ############################################ */
if (HAL_ADCEx_Calibration_Start(&AdcHandle, ADC_SINGLE_ENDED) != HAL_OK)
{
Error_Handler();
}
/* ### - 3 - Channel configuration ######################################## */
sConfig.Channel = ADC_CHANNEL_3; /* Channel to be converted */
sConfig.Rank = ADC_RANK_CHANNEL_NUMBER;
if (HAL_ADC_ConfigChannel(&AdcHandle, &sConfig) != HAL_OK)
{
Error_Handler();
}
sConfig.Channel = ADC_CHANNEL_7; /* Channel to be converted */
sConfig.Rank = ADC_RANK_CHANNEL_NUMBER;
if (HAL_ADC_ConfigChannel(&AdcHandle, &sConfig) != HAL_OK)
{
Error_Handler();
}
/* ### - 4 - Start conversion in DMA mode ################################# */
if (HAL_ADC_Start_DMA(&AdcHandle,
(uint32_t *)aADCxConvertedData, //this is my ADC data[]
ADC_CONVERTED_DATA_BUFFER_SIZE //32 but essentially 2
) != HAL_OK)
{
Error_Handler();
}
/* Infinite Loop */
while (1)
{
}
2020-08-07 6:39 AM
> When connecting to CH 3 then even number index array is 4096, others are about 3000 )
Okay. How are the other channels connected?
There is going to be some cross talk between a channel and the next converted channel. Increase sampling time to mitigate.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.