2015-06-12 7:38 AM - last edited on 2024-10-21 3:47 AM by Andrew Neil
Posted on June 12, 2015 at 16:38
If someone is interested in developing devices that use protocol MQTT leave some information about what I have done (... not my code ....my boss fire me)
In attachment the protocol specifications (I am sorry I forget where I download the document)
Here http://www.hivemq.com/downloads/
The mqtt broker for windows or linux (I work with windows version) very simpe start... ''run.bat''
Well documented conf directory contain all config parametersall well explained in site doc
The broker open the standard ports 1883 or 8000 for websockets
With wireshark you can monitor the traffic and save lot of time for debug
My wireshark version 1.12.5 support mqtt dissector and all message are full decoded
Form here: http://ftp.acc.umu.se/mirror/eclipse.org/paho/1.0/
I have downloaded org.eclipse.phao.mqtt.utility.1.0.1.jar
Small mqtt client used for subcribe topic and checking mi device mqtt publishing
#mqtt-protocol
2015-06-12 7:54 AM
Thank you for sharing your knowledge.
> ... not my code ....my boss fire me Fortunately, there is open source code available, likehttps://github.com/AvengerGear/chibios-stm32f407-discovery-mqtt
project.2015-06-12 10:09 AM - last edited on 2024-10-21 3:49 AM by Andrew Neil
Posted on June 12, 2015 at 19:09
Oh yes another source
http://git.eclipse.org/c/paho/org.eclipse.paho.mqtt.embedded-c.git/
(but not for ST)
But the code is not mine, I am paid to write it, and it does not seem correct to publish it.
I wanted to give the ''public information'' to faciltiare who will develop applications with MQTT.
I do not know if the code ready to use can be used in commercial products that do not include the release of the code.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.