cancel
Showing results for 
Search instead for 
Did you mean: 

Modifying ASC python script for Keyword spotting. getting error during log mel feature extraction. Please help

ShivaRagu
Senior

hi, am modifying the ASC python code for keyword spotting. Am using dataset which is 1 sec long wav files whereas ASC dataset is 30sec long wav files. 

while doing spectrogram-feature extraction am getting value 0.

what is the frame length and hop length I need to give for 1sec long audio?

Also, whether I can use the same log mel feature extraction module for this?

Please help.

Python Script link-

https://colab.research.google.com/drive/1lBca6J1kUTNG8MmaM_TTPV8M-5IXdy7Y#scrollTo=1pZBm4W3khO8

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Bruno_ST
ST Employee

Hi @ShivaRagu​ 

I am not the owner of that script, but the purpose is to have 1024ms frame to be in the power of 2 (to ease computation). In the script, the frame length should be adapted to 1s to fit the dataset length. Where you able to solve you issue ?

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.