2010-07-27 2:08 AM
Microcontroller Clock Output pin MCO
2011-05-17 5:00 AM
Try this (for system clock output):
g_pRCC->CFGR = MCO2; g_pRCC->APB2ENR |= IOPAEN | AFIOEN; g_pGPIOA->CRH &= ~0X0000000F; g_pGPIOA->CRH |= 0X0000000B; Created using the Crossware RCC and Ports code creation wizards.2011-05-17 5:00 AM
First of all thanks for the quick response.
/* ============================================================ *//* ============================================================ */void CLK_configuration (void) { /* ~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~ */ /* ~~~~~~~~~~~~~~~~~~~~~~~~~~ HSI RC (8 MHz) ~~~~ */ RCC_HSICmd(ENABLE); /* ENABLE/DISABLE RCC_CR.HSION - INTERNAL 8MHz OSCILLATOR ON */ while(RCC_GetFlagStatus(RCC_FLAG_HSIRDY) == RESET); /* WAIT TO HARDWARE OFF */ RCC_SYSCLKConfig(RCC_SYSCLKSource_HSI); /* MODIFICA RCC_CFGR.SW - ELIGE EL HSI COMO SYSCLK SOURCE */ /* ~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~ */ /* ~~~~~~~~~~ HSE_Value (8 MHz) stm32f10x_conf.h ~~~~ */ RCC_HSEConfig(RCC_HSE_ON); /* ON/OFF RCC_CR.HSEON - EXTERNAL 8MHz OSCILLATOR ON */ while(RCC_GetFlagStatus(RCC_FLAG_HSERDY) == RESET); /* WAIT TO HARDWARE OFF */ /* ~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~ */ /* ~~~~~~~~PHASE LOOP LOCKED PLLCLK->56MHz ~~~~ */ RCC_PLLCmd(DISABLE); /* ENABLE/DISABLE RCC_CR.PLLON */ RCC_PLLConfig(RCC_PLLSource_HSE_Div1,RCC_PLLMul_9); /* SYSCLK=72MHZ- RCC_CFGR.PLLSRC=1, RCC_CFGR.PLLXRPRE=0 y RCC_CFGR.PLLMULL=0111 */ RCC_PLLCmd(ENABLE); /* ENABLE/DISABLE RCC_CR.PLLON */ while(RCC_GetFlagStatus(RCC_FLAG_PLLRDY) == RESET); /* WAIT TO HARDWARE OFF */ /* ~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~ */ /* ~ SYSTEM CLOCK SYSCLK=72MHZ HCLK=72MHZ ~~~~ */ RCC_USBCLKConfig(RCC_USBCLKSource_PLLCLK_1Div5); /* RELOJ DEL USB - 72MHz/1.5=48MHZ */ RCC_ADCCLKConfig(RCC_PCLK2_Div8); /* RELOJ DEL ADC PCLK2/8=9MHz - CONFIGURE RCC_CFGR.ADCPRE */ RCC_PCLK2Config(RCC_HCLK_Div1); /* CONFIGURE RCC_CFGR.PPRE2 APB2 PCLK2=72MHz */ RCC_PCLK1Config(RCC_HCLK_Div2); /* CONFIGURE RCC_CFGR.PPRE1 APB1 PCLK1=36MHz */ RCC_HCLKConfig(RCC_SYSCLK_Div1); /* CONFIGURE RCC_CFGR.HPRE AHB HCLK=72MHz*/ /* ~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~ */ /* ~~~~~~~~~~~~~~~~~~~~~~~~~~~~ EMB_FLASH ~~~~ */ #ifdef EMB_FLASH // 5. Init Embedded Flash // Zero wait state, if 0 < HCLK 24 MHz // One wait state, if 24 MHz < HCLK 56 MHz // Two wait states, if 56 MHz < HCLK 72 MHz // Flash wait state FLASH_SetLatency(FLASH_Latency_2); // Half cycle access FLASH_HalfCycleAccessCmd(FLASH_HalfCycleAccess_Disable); // Prefetch buffer FLASH_PrefetchBufferCmd(FLASH_PrefetchBuffer_Enable); #endif // EMB_FLASH /* ~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~ */ // 5. Clock system from PLL RCC_SYSCLKConfig(RCC_SYSCLKSource_PLLCLK); /* SELECCIONA EL CLOCK DEL PLL - MODIFICA RCC_CFGR.SW */ }/* ============================================================ */
/* ============================================================ */void GPIO_configuration(void) { GPIO_InitTypeDef GPIO_InitStructure; /* ~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~ */ /* ~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~ GPIO INIT ~~~ */ #define sysclk 0x04000000
#define HSIclk 0x05000000
#define HSEclk 0x06000000
#define PLLdiv2 0x07000000 /* ~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~ */ /* ~~~~~ OUTPUT PINS ~~~~~ */ RCC_APB2PeriphClockCmd(RCC_APB2Periph_GPIOA,ENABLE); /* ENABLE CLK PORTS */ RCC_APB2PeriphResetCmd(RCC_APB2Periph_GPIOA,DISABLE); /* NO RESET PORTS */ GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz; /* MAX VEL ESCRITURA */ GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF_PP; /* ALTERNATE OUTPUT PUSH-PULL */ GPIO_InitStructure.GPIO_Pin = GPIO_Pin_8; GPIO_Init(GPIOA, &GPIO_InitStructure); RCC->CFGR |= sysclk; } /* ~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~ */ /* ~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~ */ I configure the PA.8 pin as ALTERNATE OUTPUT PUSH-PULL like RM0008 on pag 147. Then I configure RCC_CFGR.MCO with some diferents values to watch the microcontroller clock output, like RM0008 in pag 85. I´m doing well?? I see on oscilloscope the sysclk signal to 72MHz. It varies between 71,70Mhz to 72,70MHz in instant measures, and in average mode, i see 72,30MHz. Is it normal??
2011-05-17 5:00 AM
Yes. All PLL's have some ''jitter''. That's what you're seeing.
2011-05-17 5:00 AM
Thks for replying.
2011-05-17 5:00 AM
Dear diez,
This is to let you know that your exceeding the MCO Output maximum Frequency and you running it out of the specification. The maximum output of our MCO is limited to 50Mhz only as any I/O. Please refer to Datasheet, Section - Table : '' I/O AC characteristics''. Regards, STOne-32.2011-05-17 5:00 AM
2011-05-17 5:00 AM
Yes but you were complaining about jitter. You can't complain about performance (or expect any reliability -- especially across multiple parts) if you are running outside of specification.
2011-05-17 5:00 AM
Hi diez,
I'm a little confused about what you are asking. Are you asking if the variance you are seeing is normal OR are you asking if 72MHz is normal. If you didn't expect to see 72MHz what frequency were you expecting to see? Regards Trevor2011-05-17 5:00 AM
You should be using
RCC_MCOConfig
() with the RCC_MCO_PLLCLK_Div2 argument to get a 36MHz output on PA8. I assume you used RCC_MCO_SYSCLK instead (i.e. 72MHz). I'm sure the waveform you're getting in more sine that square. ST-One is correct you should not output more than 50MHz to a port pin as the rise-fall times will distort the waveform.We’re moving the ST Community to a new platform to give you a better and more reliable community experience.