2009-01-27 9:09 AM
Maximum Watchdog Time-Out
2011-05-17 4:00 AM
Reading RM0008 it seems that the maximum time-out for the watchdog timer is 58 ms. Is that correct? Can it be expanded to 1 or 2 seconds?
This is a very small value, most other products give a much broader range of values. We have library functions that take more than 58 ms, and with this short time-out value we will have sprinkle watchdog hits into the library functions. Servicing the watchdog in an intterupt seems to defeat the function.2011-05-17 4:00 AM
The max is 26 seconds not 58mS. I use this:
Code:
static void start_watchdog(void) { RCC_LSICmd( ENABLE ); // enable low speed internal clock used by watchdog while (IWDG->SR & 0x3); // wait for previos update operations to complete IWDG->KR = 0x5555; // Enable independent watchdog register access IWDG->PR = 6; // prescaller set to divice by 256 (min 6.4ms, max 26214.4ms) IWDG->RLR = 0xFFF; // reload value (0xFFF max) IWDG->KR = 0xCCCC; // start the watchdog } void stroke_watchdog(void) { IWDG->KR = 0xAAAA; } Regards Trevor2011-05-17 4:00 AM
Thanks, I had overlooked the IWDG and focusing on the WWDB.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.