2022-03-02 3:25 AM
Hi,
I have questions about LSE Drive (STM32L0).
1) In RCC register are LSEDRV[1:0] bits and I am not sure if I understand it corretly.
From datasheet about these bits: They are cleared by a power-on reset or an RTC reset. Once “00�? has been written, the content of LSEDRV cannot be changed by software.
It means once I set them to zero then I can not change it in SW again?
2) My crystal has only params like: ESR, DriveLevel (min,max), Cshunt, Cload. How Can I calculate drive level when I do not know nothing about Gmcritical_max, also I do not have current probe to measure current in crystal?
Thank you very much. Jan.
Solved! Go to Solution.
2022-03-07 9:33 AM
Hi,
1) As mentioned in Reference manual RM0377 Rev 10 section 7.2.5 LSE clock, The crystal oscillator driving strength can be changed at runtime through the LSEDRV[1:0]. So, you can change it by software.
I will rise an internal request to remove this note (They are cleared by a power-on reset or an RTC reset. Once “00�? has been written, the content of LSEDRV cannot be changed by software) from reference manual.
2) Please refer to AN2867 "Oscillator design guide for STM8AF/AL/S, STM32 MCUs and MPUs "to calculate gmcrit(crystal) and compare it with Gmcrit_max(MCU). Special focus on sections 3.3 Load capacitance and 3.4 Oscillator transconductance.
Bouraoui
2022-03-07 9:33 AM
Hi,
1) As mentioned in Reference manual RM0377 Rev 10 section 7.2.5 LSE clock, The crystal oscillator driving strength can be changed at runtime through the LSEDRV[1:0]. So, you can change it by software.
I will rise an internal request to remove this note (They are cleared by a power-on reset or an RTC reset. Once “00�? has been written, the content of LSEDRV cannot be changed by software) from reference manual.
2) Please refer to AN2867 "Oscillator design guide for STM8AF/AL/S, STM32 MCUs and MPUs "to calculate gmcrit(crystal) and compare it with Gmcrit_max(MCU). Special focus on sections 3.3 Load capacitance and 3.4 Oscillator transconductance.
Bouraoui
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.