2025-07-29 3:42 AM
I'm using the STM32U031C8U6 with STM32CubeIDE 1.19.0 and can't figure out how LPTIM1 works.
I created a new project and enabled LPTIM1 in Device Configuration Tools (Mode: Counts internal clock events). In the NVIC Interrupt table tab, I enabled the interrupt.
In Clock Configuration, I enabled LSE clock (32768 kHz) and selected it on the LTPIM1 Clock Mux.
I generated the code and modified the main() function as follows:
int main(void)
{
HAL_Init();
SystemClock_Config();
MX_GPIO_Init();
MX_LPTIM1_Init();
HAL_LPTIM_TimeOut_Start_IT(&hlptim1, 320);
while (1)
{
HAL_PWR_EnterSTOPMode(PWR_LOWPOWERREGULATOR_ON, PWR_STOPENTRY_WFI);
}
}HAL_LPTIM_TimeOut_Start_IT() enables the timeout function, sets compare register CCR1 = 320 and starts the timer in continuous mode.
I expected the HAL_LPTIM_CompareMatchCallback callback to be called every 10 ms (320 / 32768 kHz), waking up the micro.
This callback is actually triggered every 2 seconds according the value of the ARR register (by default, 65535).
I verified that the frequency with which the callback is called depends on the ARR register by trying different values.
Can anyone explain to me why the HAL_LPTIM_CompareMatchCallback() isn't called when the CNT == CCR1?
And why is it called when CNT == ARR? In this case I would have expected the triggering of HAL_LPTIM_AutoReloadMatchCallback().
Thank you in advance,
G.
Solved! Go to Solution.
2025-07-29 6:35 AM
You didn't show your callback function, but I'm guessing it doesn't take any action.
I think the notion behind this mechanism is that a timeout (callback) is a significant event, and the callback will take some action, e.g. report the timeout, then reset the counter (COUNTRST, e.g.) for the next timeout. Otherwise (in the absence of a trigger event) the counter will just keep counting until it wraps at ARR, yielding a callback period of =ARR.
2025-07-29 6:10 AM
There is a single counter per timer that counts from 0 to ARR. If you want to change the timer update frequency, change ARR, not CCRx.
HAL_LPTIM_CompareMatchCallback is called when CNT = CCRx.
2025-07-29 6:35 AM
You didn't show your callback function, but I'm guessing it doesn't take any action.
I think the notion behind this mechanism is that a timeout (callback) is a significant event, and the callback will take some action, e.g. report the timeout, then reset the counter (COUNTRST, e.g.) for the next timeout. Otherwise (in the absence of a trigger event) the counter will just keep counting until it wraps at ARR, yielding a callback period of =ARR.
2025-07-29 6:35 AM
I understood what my mistake was: inside HAL_LPTIM_CompareMatchCallback I did not reset the counter so this is actually triggeed with the frequency depending on ARR.
Thank you,
G.
2025-07-29 6:47 AM
I just found the problem a little while ago. Thanks a lot anyway,
G.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.