2010-12-27 11:53 PM
Hello,
I'm trying to run WC1602A LCD display but nothing happens, can anyone pinpoint me where i have a mistake in code (the code is compiling) because i was analising it whole night and couldn't find one
int main(void)
{
LCD_Init();
LCD_Clear();
LCD_GoTo(0,0);
LCD_SendText(''Hello\0'');
STM32vldiscovery_LEDInit(LED3);
STM32vldiscovery_LEDInit(LED4);
STM32vldiscovery_PBInit(BUTTON_USER, BUTTON_MODE_GPIO);
}
lcd4bit.h
#include ''stm32f10x.h''
#define LCD_D4 GPIO_Pin_3 // PC3
#define LCD_D5 GPIO_Pin_2 // PC2
#define LCD_D6 GPIO_Pin_1 // PC1
#define LCD_D7 GPIO_Pin_0 // PC0
#define LCD_D_ALL GPIO_Pin_3 & GPIO_Pin_2 & GPIO_Pin_1 & GPIO_Pin_0 //GPIO_Pin_All // PC0, PC1, PC2, PC3
#define LCD_RS GPIO_Pin_12 // PC12
#define LCD_RW GPIO_Pin_11 // PC11
#define LCD_EN GPIO_Pin_10 // PC10
void delay_ms(int ms);
void delay_us(int us);
uint8_t LCD_ReadByte(void);
void LCD_SendByte(uint8_t cmd);
void LCD_SendCmd (uint8_t cmd);
void LCD_SendData(uint8_t data);
void LCD_SendText(uint8_t * text);
void LCD_GoTo (uint8_t wers, uint8_t kol);
void LCD_Clear (void);
void LCD_Init (void);
lcd4bit.c
#include ''lcd4bit.h''
//====================================
void delay_ms(int ms)
{
int i, tms;
tms = 9000*ms;
for(i=0;i<tms;i++);
}
//======================================
void delay_us(int us)
{
int i, tus;
tus = 9*us;
for(i=0;i<tus;i++);
}
//=======================================================
uint8_t LCD_ReadByte(void)
{
GPIO_InitTypeDef GPIO_Conf;
uint8_t ReadedData=0;
GPIO_SetBits(GPIOC, LCD_D_ALL);
// Zmiana konfiguracji wyprowadzen na wejsciach
GPIO_Conf.GPIO_Pin = GPIO_Pin_0 | GPIO_Pin_1 | GPIO_Pin_2 | GPIO_Pin_3;
GPIO_Conf.GPIO_Mode = GPIO_Mode_IN_FLOATING;
GPIO_Conf.GPIO_Speed = GPIO_Speed_50MHz;
GPIO_Init(GPIOC, &GPIO_Conf);
GPIO_SetBits(GPIOC, LCD_RW);
GPIO_SetBits(GPIOC, LCD_EN);
if(GPIO_ReadInputDataBit(GPIOC, LCD_D7)) //odczyt starszej polowy
ReadedData |= 0x80;
if(GPIO_ReadInputDataBit(GPIOC, LCD_D6))
ReadedData |= 0x40;
if(GPIO_ReadInputDataBit(GPIOC, LCD_D5))
ReadedData |= 0x20;
if(GPIO_ReadInputDataBit(GPIOC, LCD_D4))
ReadedData |= 0x10;
GPIO_ResetBits(GPIOC, LCD_EN);
delay_us(30);
GPIO_SetBits(GPIOC, LCD_EN);
if(GPIO_ReadInputDataBit(GPIOC, LCD_D7)) //odczyt mlodszej polowy
ReadedData |= 0x08;
if(GPIO_ReadInputDataBit(GPIOC, LCD_D6))
ReadedData |= 0x04;
if(GPIO_ReadInputDataBit(GPIOC, LCD_D5))
ReadedData |= 0x02;
if(GPIO_ReadInputDataBit(GPIOC, LCD_D4))
ReadedData |= 0x01;
GPIO_ResetBits(GPIOC, LCD_EN);
// Powrot do pierwotnych ustawien wyprowadzen
GPIO_Conf.GPIO_Pin = GPIO_Pin_0 | GPIO_Pin_1 | GPIO_Pin_2 | GPIO_Pin_3;
GPIO_Conf.GPIO_Mode = GPIO_Mode_Out_PP;
GPIO_Conf.GPIO_Speed = GPIO_Speed_50MHz;
GPIO_Init(GPIOC, &GPIO_Conf);
return ReadedData;
}
//=============================================================================
void LCD_SendByte(uint8_t cmd)
{
uint8_t tcmd = 0;
GPIO_ResetBits(GPIOC, LCD_RW);
GPIO_ResetBits(GPIOC, LCD_D_ALL);
GPIO_SetBits(GPIOC, LCD_EN);
tcmd = cmd >> 4; // 4x w prawo
if( tcmd & 0x01 )
GPIO_SetBits(GPIOC, LCD_D4); //zapis starszej polowy
if( tcmd & 0x02 )
GPIO_SetBits(GPIOC, LCD_D5);
if( tcmd & 0x04 )
GPIO_SetBits(GPIOC, LCD_D6);
if( tcmd & 0x08 )
GPIO_SetBits(GPIOC, LCD_D7);
GPIO_ResetBits(GPIOC, LCD_EN);
delay_us(30);
GPIO_SetBits(GPIOC, LCD_EN);
GPIO_ResetBits(GPIOC, LCD_D_ALL);
cmd &= 0x0F; // maskowanie czterech mlodszych bitow
if( cmd & 0x01 )
GPIO_SetBits(GPIOC, LCD_D4); //zapis mlodszej polowy
if( cmd & 0x02 )
GPIO_SetBits(GPIOC, LCD_D5);
if( cmd & 0x04 )
GPIO_SetBits(GPIOC, LCD_D6);
if( cmd & 0x08 )
GPIO_SetBits(GPIOC, LCD_D7);
GPIO_ResetBits(GPIOC, LCD_EN);
GPIO_ResetBits(GPIOC, LCD_D_ALL);
GPIO_ResetBits(GPIOC, LCD_RS);
while(LCD_ReadByte() & 0x80); // czekaj na zakonczenie operacji
}
//============================================================================
void LCD_SendCmd(uint8_t cmd)
{
GPIO_ResetBits(GPIOC, LCD_RS);
LCD_SendByte(cmd);
}
//=============================================================================
void LCD_SendData(uint8_t data)
{
GPIO_SetBits(GPIOC, LCD_RS);
LCD_SendByte(data);
}
//===============================================================================
void LCD_SendText(uint8_t * text)
{
while(*text)
{
LCD_SendData(*text);
text++;
}
}
//=======================================================================================
void LCD_Clear(void)
{
LCD_SendCmd(0x01);
}
//=====================================================================================
void LCD_GoTo(uint8_t wers, uint8_t kol)
{
uint8_t pos = 0;
pos = (wers * 0x40) + kol;
pos += 0x80;
LCD_SendCmd(pos);
}
//===========================================================================
void LCD_Init(void)
{
uint8_t i;
GPIO_InitTypeDef GPIO_Conf;
RCC_APB2PeriphClockCmd(RCC_APB2Periph_GPIOC, ENABLE);
GPIO_Conf.GPIO_Pin = GPIO_Pin_0 | GPIO_Pin_1 | GPIO_Pin_2 | GPIO_Pin_3 | GPIO_Pin_10 | GPIO_Pin_11 | GPIO_Pin_12;
GPIO_Conf.GPIO_Mode = GPIO_Mode_Out_PP;
GPIO_Conf.GPIO_Speed = GPIO_Speed_50MHz;
GPIO_Init(GPIOC, &GPIO_Conf);
delay_ms(30); //me
GPIO_ResetBits(GPIOC, LCD_RS);
GPIO_ResetBits(GPIOC, LCD_EN);
for(i = 0; i<3; i++)
{
GPIO_SetBits(GPIOC, LCD_EN);
GPIO_SetBits(GPIOC, LCD_D4 | LCD_D5);
GPIO_ResetBits(GPIOC, LCD_D6 | LCD_D7);
GPIO_ResetBits(GPIOC, LCD_EN);
delay_ms(5);
}
GPIO_SetBits(GPIOC, LCD_EN);
GPIO_SetBits(GPIOC, LCD_D5);
GPIO_ResetBits(GPIOC,LCD_D4 | LCD_D6 | LCD_D7);
GPIO_ResetBits(GPIOC, LCD_EN);
LCD_SendCmd(0x28);
LCD_SendCmd(0x08);
LCD_SendCmd(0x01);
LCD_SendCmd(0x06);
LCD_SendCmd(0x0C);
delay_ms(5); //me
}
2010-12-28 9:01 AM
Hi bartek;
I think your mistake comes from the following line: #define LCD_D_ALL GPIO_Pin_3 & GPIO_Pin_2 & GPIO_Pin_1 & GPIO_Pin_0 //GPIO_Pin_All // PC0, PC1, PC2, PC3 it should be: #define LCD_D_ALL (GPIO_Pin_3 | GPIO_Pin_2 | GPIO_Pin_1 | GPIO_Pin_0) B.R. STM322010-12-29 4:27 AM
2010-12-29 12:26 PM
I already did that but that wasn't a solution, still nothing happend with LCD
May be you got it wired wrong. Without knowing what you've wired where it's hard to say. Break out the scope and look at the signals, and debug it. Start with some simple interactions with the LCD and work from there.2010-12-30 2:37 AM
Hi Bartek,
try it: main: LCD_Init(); LCD_Clear(); LCD_GoTo(0,0); //LCD_SendCmd(0x02); //home delay_ms(5); LCD_SendText(''Hello''); LCD:#define LCD_D4 GPIO_Pin_3 // PC3 #define LCD_D5 GPIO_Pin_2 // PC2 #define LCD_D6 GPIO_Pin_1 // PC1 #define LCD_D7 GPIO_Pin_0 // PC0 #define LCD_D_ALL (GPIO_Pin_3 | GPIO_Pin_2 | GPIO_Pin_1 | GPIO_Pin_0) //GPIO_Pin_All // PC0, PC1, PC2, PC3 #define LCD_RS GPIO_Pin_12 // PC12 //#define LCD_RW GPIO_Pin_11 // PC11 #define LCD_EN GPIO_Pin_11 // PC11 void delay_ms(int ms); void delay_us(int us); //uint8_t LCD_ReadByte(void); void LCD_SendByte(uint8_t cmd); void LCD_SendCmd (uint8_t cmd); void LCD_SendData(uint8_t data); void LCD_SendText(uint8_t * text); void LCD_GoTo (uint8_t wers, uint8_t kol); void LCD_Clear (void); void LCD_Init (void); //==================================== void delay_ms(int ms) { int i, tms; tms = 9000*ms; for(i=0;i<tms;i++); } //====================================== void delay_us(int us) { int i, tus; tus = 9*us; for(i=0;i<tus;i++); } //============================================================================= void LCD_SendByte(uint8_t cmd) { uint8_t tcmd = 0; GPIO_ResetBits(GPIOC, LCD_D_ALL); tcmd = cmd >> 4; // 4x w prawo if( tcmd & 0x01 ) GPIO_SetBits(GPIOC, LCD_D4); //zapis starszej polowy if( tcmd & 0x02 ) GPIO_SetBits(GPIOC, LCD_D5); if( tcmd & 0x04 ) GPIO_SetBits(GPIOC, LCD_D6); if( tcmd & 0x08 ) GPIO_SetBits(GPIOC, LCD_D7); GPIO_SetBits(GPIOC, LCD_EN); //E pulse delay_us(30); GPIO_ResetBits(GPIOC, LCD_EN); GPIO_ResetBits(GPIOC, LCD_D_ALL); cmd &= 0x0F; // maskowanie czterech mlodszych bitow if( cmd & 0x01 ) GPIO_SetBits(GPIOC, LCD_D4); //zapis mlodszej polowy if( cmd & 0x02 ) GPIO_SetBits(GPIOC, LCD_D5); if( cmd & 0x04 ) GPIO_SetBits(GPIOC, LCD_D6); if( cmd & 0x08 ) GPIO_SetBits(GPIOC, LCD_D7); GPIO_SetBits(GPIOC, LCD_EN); //E pulse delay_us(30); GPIO_ResetBits(GPIOC, LCD_EN); GPIO_ResetBits(GPIOC, LCD_D_ALL); GPIO_ResetBits(GPIOC, LCD_RS); delay_us(200); //while(LCD_ReadByte() & 0x80); // czekaj na zakonczenie operacji } //============================================================================ void LCD_SendCmd(uint8_t cmd) { GPIO_ResetBits(GPIOC, LCD_RS); LCD_SendByte(cmd); } //============================================================================= void LCD_SendData(uint8_t data) { GPIO_SetBits(GPIOC, LCD_RS); LCD_SendByte(data); } //=============================================================================== void LCD_SendText(uint8_t * text) { while(*text) { LCD_SendData(*text); text++; } } //======================================================================================= void LCD_Clear(void) { LCD_SendCmd(0x01); delay_ms(5); } //===================================================================================== void LCD_GoTo(uint8_t wers, uint8_t kol) { uint8_t pos = 0; pos = (wers * 0x40) + kol; pos += 0x80; LCD_SendCmd(pos); } //=========================================================================== void LCD_Init(void) { uint8_t i; GPIO_InitTypeDef GPIO_Conf; RCC_APB2PeriphClockCmd(RCC_APB2Periph_GPIOC, ENABLE); GPIO_Conf.GPIO_Pin = GPIO_Pin_0 | GPIO_Pin_1 | GPIO_Pin_2 | GPIO_Pin_3 | GPIO_Pin_10 | GPIO_Pin_11 | GPIO_Pin_12; GPIO_Conf.GPIO_Mode = GPIO_Mode_Out_PP; GPIO_Conf.GPIO_Speed = GPIO_Speed_50MHz; GPIO_Init(GPIOC, &GPIO_Conf); delay_ms(30); //me GPIO_ResetBits(GPIOC, LCD_RS); GPIO_ResetBits(GPIOC, LCD_EN); for(i = 0; i<3; i++) { GPIO_SetBits(GPIOC, LCD_EN); GPIO_SetBits(GPIOC, LCD_D4 | LCD_D5); GPIO_ResetBits(GPIOC, LCD_D6 | LCD_D7); GPIO_ResetBits(GPIOC, LCD_EN); delay_ms(5); } GPIO_SetBits(GPIOC, LCD_EN); GPIO_SetBits(GPIOC, LCD_D5); GPIO_ResetBits(GPIOC,LCD_D4 | LCD_D6 | LCD_D7); GPIO_ResetBits(GPIOC, LCD_EN); LCD_SendCmd(0x28); LCD_SendCmd(0x08); LCD_SendCmd(0x01); delay_ms(5); LCD_SendCmd(0x06); LCD_SendCmd(0x0C); delay_ms(5); //me } You haven't to wait for reply from LCD at end of sending data - delay is enough. Also I improve delays and E-pulses. It work on my board. Regards, MHWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.