2012-12-12 1:09 AM
I am trying to use an LCD HD44780 (2X40) with STM3210C-eval. I want to configure it for 8 bits mode.
#re-inventing-the-wheel2013-01-02 1:10 AM
finally, it works with 4bits-mode.
thank you for yor help. :)2013-01-02 8:29 AM
Glad for that - congrats!
It would be most helpful to the (exhausted) yet interested others who read this - if you'd detail just how you finally succeeded. Suspect (as always) that ''initialization'' was key - and that once this was solved you could work out the dual nibble, character entry details...2013-01-08 7:28 AM
I increase the time of delay (<<2) in lcd_init .
I Minimize the cable length between the module and host MPU. (Recommended max. length 30 cm). also I find that the lcd need negative votlage Max(VDD-Vo)=13.2013-01-08 7:42 AM
Glad you persisted - got it working.
Very early on - you were advised about likely need for negative voltage @ Vo pin. However - we know of NO 2 line, character display - that requires up to -8V (wrt gnd) on Vo. Suspect yours operates quite well w/ -2, -3 max @ Vo. So long as you follow the initialization delay details outlined here (w/real values) - you should be ok. The very first initialization codes require unusually long delays - after those things become more reasonable. When using 4 bit mode - always advisable to periodically, ''re-initialize'' the Lcd - just in case noise or power issue has caused the Lcd to become, ''disordered.''We’re moving the ST Community to a new platform to give you a better and more reliable community experience.