2015-07-09 1:30 AM
I work on a project ''distance meter kit '' Here is the link.
http://asv-lab.ru/blog/fazovyj_lazernyj_dalnomer_asv50m/2015-06-26-12
There are videos. In the comments under the video link to the file excel. This file is recorded measurement phase at a frequency of 45 MHz, 30 MHz, 3 MHz. Measurement of the phase increments of 100 millimeters. From the values of the phase, we can calculate the distance. 45 MHz Phase 0-360 = 3,75M. 30 MHz Phase 0-360 = 5M. 3 MHz Phase 0-360 = 50M I have a problem at the time of the transition phase from 0 to 360 or 360 to 0. It is not always properly defined range 0-3,75m or 3,75-7,5m Help calculate. thank.2015-07-09 8:01 AM
The first measurement for 2700 mm seems a bit bogus. Like it's 60 degrees off
Not sure what the scope of the phase is here, assuming the phase is 16-bit, so each tick is 360/65536I'm going to guess you're doing an average, and when your floating in the 0 degrees region, you get some measurements (or a measurement) in the 65500 ish range and you're adding that in, skewing the numbers, instead of recognizing it as a negative number and subtracting 65536 from it to place it in the prior cycle instead of the current one.2015-07-09 8:17 AM
tick = 1/120000000;
interfal = 655350;average = 10;phase f1-f2 = 11,7358;Khz2016-01-26 8:09 AM
sorry for my bad English.
I corrected the algorithm. The phase measurement 45 MHz and 3 MHz at a distance of 30 meters 1 step 20mm 1500 points. 3 MHz for calculating the multiplier i.ph_long = ph45Mhz+360*i The source code below how to do this correctly?
[code]if ((phase3Mhz_deg > 33000) || (phase3Mhz_deg < 300)) {
coefmux = 1;
} else if ((phase3Mhz_deg >= 300) && (phase3Mhz_deg < 1100)) {
if (phase45Mhz_deg > 18000) {
coefmux = 1;
} else {
coefmux = 2;
}
} else if ((phase3Mhz_deg >= 1100) && (phase3Mhz_deg < 3100)) {
coefmux = 2;
} else if ((phase3Mhz_deg >= 3100) && (phase3Mhz_deg < 4100)) {
if (phase45Mhz_deg > 18000) {
coefmux = 2;
} else {
coefmux = 3;
}
} else if ((phase3Mhz_deg >= 4100) && (phase3Mhz_deg < 5100)) {
coefmux = 3;
} else if ((phase3Mhz_deg >= 5100) && (phase3Mhz_deg < 6400)) {
if (phase45Mhz_deg > 18000) {
coefmux = 3;
} else {
coefmux = 4;
}
} else if ((phase3Mhz_deg >= 6400) && (phase3Mhz_deg < 8300)) {
coefmux = 4;
} else if ((phase3Mhz_deg >= 8300) && (phase3Mhz_deg < 8900)) {
if (phase45Mhz_deg > 18000) {
coefmux = 4;
} else {
coefmux = 5;
}
} else if ((phase3Mhz_deg >= 8900) && (phase3Mhz_deg < 10700)) {
coefmux = 5;
} else if ((phase3Mhz_deg >= 10700) && (phase3Mhz_deg < 11500)) {
if (phase45Mhz_deg > 18000) {
coefmux = 5;
} else {
coefmux = 6;
}
} else if ((phase3Mhz_deg >= 11500) && (phase3Mhz_deg < 13000)) {
coefmux = 6;
} else if ((phase3Mhz_deg >= 13000) && (phase3Mhz_deg < 14000)) {
if (phase45Mhz_deg > 18000) {
coefmux = 6;
} else {
coefmux = 7;
}
} else if ((phase3Mhz_deg >= 14000) && (phase3Mhz_deg < 15500)) {
coefmux = 7;
} else if ((phase3Mhz_deg >= 15500) && (phase3Mhz_deg < 16500)) {
if (phase45Mhz_deg > 18000) {
coefmux = 7;
} else {
coefmux = 8;
}
} else if ((phase3Mhz_deg >= 16500) && (phase3Mhz_deg < 18000)) {
coefmux = 8;
} else if ((phase3Mhz_deg >= 18000) && (phase3Mhz_deg < 19300)) {
if (phase45Mhz_deg > 18000) {
coefmux = 8;
} else {
coefmux = 9;
}
} else if ((phase3Mhz_deg >= 19300) && (phase3Mhz_deg < 20400)) {
coefmux = 9;
} else if ((phase3Mhz_deg >= 20400) && (phase3Mhz_deg < 21700)) {
if (phase45Mhz_deg > 18000) {
coefmux = 9;
} else {
coefmux = 10;
}
} else if ((phase3Mhz_deg >= 21700) && (phase3Mhz_deg < 23000)) {
coefmux = 10;
} else if ((phase3Mhz_deg >= 23000) && (phase3Mhz_deg < 24500)) {
if (phase45Mhz_deg > 18000) {
coefmux = 10;
} else {
coefmux = 11;
}
} else if ((phase3Mhz_deg >= 24500) && (phase3Mhz_deg < 26500)) {
coefmux = 11;
} else {
coefmux = 0;
}
tempdouble = 36000.0 * (coefmux - 1.0) + phase45Mhz_deg;
ph_long = floor(tempdouble);
[/code]File with the measurement results.https://drive.google.com/file/d/0B3blsgr5W0tTWm1menI4eHctNkU/view?usp=sharing
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.