2014-02-27 2:41 AM
keil 5.10 does not support STM32 firmware library, is there any way to use keil 5.xx with STM32 driver library?
2014-02-28 12:03 AM
I also found this problem. I asked Keil who replied,
''Yes, there are conflicts in our drivers and the ST library. I think the basic idea to work around this problem is to clearly separate the source code into parts that USE_STDPERIPH_DRIVER and the part that does not USE_STDPERIPH_DRIVER, which includes the RTE code. In uVision you can use source groups for this type of separation. So do not globally enable USE_STDPERIPH_DRIVER in your project, but only in the modules (source groups) that really use the ST library.'' I have not tried this as I have gone back to using MDK 4 for the moment.2014-03-15 5:54 PM
Try this
http://www2.keil.com/mdk5/legacy ''MDK Version 5 - Legacy Support MDK Version 5 uses Software Packs to support a microcontroller device and to use middleware. To maintain backward compatibility with MDK Version 4 you may install Legacy Support. This might be necessary for two reasons: To maintain projects created with MDK Version 4 without migrating to Software Packs. To use devices that are not yet supported by a Device Family Pack.''We’re moving the ST Community to a new platform to give you a better and more reliable community experience.