2023-07-17 6:22 AM
I'm currently using a STM32 Nucleo-G071RB, I am trying to connect to a DAC (MCP4725) and also to a MLX90393 both using I2C, the DAC is connecting fine, but I am getting nothing from the MLX90393, has anyone used this device and been able to get anything back?
2023-07-17 7:18 AM - edited 2023-07-17 7:28 AM
Hello @JNava.3 ,
Make sur that you are using the right address and respecting the max frequency.
To check if target device is ready for communication, use the function HAL_I2C_IsDeviceReady()
Take an oscilloscope to check SDA and SCL behavior.
Foued
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.