2017-08-09 10:41 AM
Hi
First I will give info about my project.
I am generating PWM using timer, then SPI using Full Duplex slave mode and a GPIO pin.
PWM is connected to SPI sclk and GPIO is connected to NSS.
I am transferring data from 1 to 550 and 1100 to 1650. Now the problem is the first block of data i.e 1 to 550 going well. when I restart the SPI transfer I see some 2 bytes of junk data that is transferring through SPI. Below is the code and waveform.
Please suggest me and let me know where I am going wrong.
MX_GPIO_Init();
MX_DMA_Init(); MX_SPI1_Init(); MX_TIM3_Init();/* USER CODE BEGIN 2 */
int j = 1;
for (uint16_t i = 0; i < 1100; i = i+2) { testDataToSend[i] = j; testDataToSend[i+1] = j >> 8; j++; } HAL_GPIO_WritePin(GPIOA, GPIO_PIN_0, GPIO_PIN_SET); HAL_SPI_Transmit_DMA(&hspi1, testDataToSend, 1100); HAL_TIM_PWM_Start(&htim3, TIM_CHANNEL_4); HAL_Delay(1); HAL_TIM_Base_Start_IT(&htim3);while(flag != 1){
} flag = 0; for (uint16_t i = 0; i < 75; i++); HAL_GPIO_WritePin(GPIOA, GPIO_PIN_0, GPIO_PIN_SET); HAL_SPI_DMAStop(&hspi1); HAL_SPI_Abort(&hspi1); *testDataToSend = NULL;j = 1100;
for (uint16_t i = 0; i < 1100; i = i+2) { testDataToSend_1[i] = j; testDataToSend_1[i+1] = j >> 8; j++; } HAL_GPIO_WritePin(GPIOA, GPIO_PIN_0, GPIO_PIN_SET);HAL_SPI_Transmit_DMA(&hspi1, testDataToSend_1, 1100); HAL_TIM_Base_Start_IT(&htim3); while(flag != 1){ } flag = 0; for (uint16_t i = 0; i < 35; i++); HAL_GPIO_WritePin(GPIOA, GPIO_PIN_0, GPIO_PIN_SET); *testDataToSend_1 = NULL;/* USER CODE END 2 */
/* Infinite loop */
/* USER CODE BEGIN WHILE */ while (1) {}
/* USER CODE END WHILE */void DMA1_Channel3_IRQHandler(void)
{ /* USER CODE BEGIN DMA1_Channel3_IRQn 0 */flag = 1;
/* USER CODE END DMA1_Channel3_IRQn 0 */ HAL_DMA_IRQHandler(&hdma_spi1_tx); /* USER CODE BEGIN DMA1_Channel3_IRQn 1 *//* USER CODE END DMA1_Channel3_IRQn 1 */
}void TIM3_IRQHandler(void){ /* USER CODE BEGIN TIM3_IRQn 0 */HAL_GPIO_WritePin(GPIOA, GPIO_PIN_0, GPIO_PIN_RESET);
HAL_TIM_Base_Stop_IT(&htim3); /* USER CODE END TIM3_IRQn 0 */ HAL_TIM_IRQHandler(&htim3); /* USER CODE BEGIN TIM3_IRQn 1 *//* USER CODE END TIM3_IRQn 1 */
}We’re moving the ST Community to a new platform to give you a better and more reliable community experience.