2024-05-16 12:48 AM - last edited on 2024-05-16 1:16 AM by mƎALLEm
Hello ST community,
I am currently programming an ECU system, using f446re nucleo board. Right now i am trying to communicate with BMS using CAN communication.
So far, everything has been set: CAN Initialization and start, sending works properly.
The issue i am facing is that i cannot receive frames from battery, even though i can communicate with laptop for UDS protocole (Reception works properly in that case), but when i try with the battery, the debug mode doesn't stop at the rx interrupt routine.
I have verified the CANFilter configuration to make sure, i didn't see any mistake, nothing has been changed but i only can communicate with UDS frames and not with batteries.
for example: frame ID 0x586 entering fifo0 with such a filter:
void CAN_Filter_FIFO0(CAN_HandleTypeDef* hcan)
{
CAN_FilterTypeDef canfilterconfig;
canfilterconfig.FilterActivation = CAN_FILTER_ENABLE;
canfilterconfig.FilterBank = 10;
canfilterconfig.FilterFIFOAssignment = CAN_FILTER_FIFO0;
canfilterconfig.FilterIdHigh = 0x580 << 5; // According to the DBC
canfilterconfig.FilterIdLow = 0x0000;
canfilterconfig.FilterMaskIdHigh = 0xfe0<<5;// Calculation of the mask according to the DBC
canfilterconfig.FilterMaskIdLow = 0x0000;
canfilterconfig.FilterMode = CAN_FILTERMODE_IDMASK;
canfilterconfig.FilterScale = CAN_FILTERSCALE_32BIT;
canfilterconfig.SlaveStartFilterBank = 13;
HAL_CAN_ConfigFilter(hcan, &canfilterconfig);
}Please let me know if anyone has any idea.
Solved! Go to Solution.
2024-05-21 6:11 AM
Alright, found the problem, I was using both fifo0 and fifo1 for receiving whereas i had to use only one for all the frames. Don't know how to use both of them s
void HAL_CAN_RxFifo0MsgPendingCallback(CAN_HandleTypeDef *hcan)
{
HAL_CAN_GetRxMessage(&hcan1, CAN_RX_FIFO0, &RxHeader, RxFrame);
{
switch(RxHeader.StdId)
{
case 0x586:
BatteryChargeCurrent_rcv(RxFrame, &rx_BCC); //Receive frame
BatteryChargeCurrent_memHandler(rx_BCC, &h_BCC); //handle memory
BCCFlag++;
break;
case 0x591:
BatteryCurrentLimit_rcv(RxFrame, &rx_BCL); //Receive frame
BatteryCurrentLimit_memHandler(rx_BCL, h_BCL); //handle memory
BCLFlag++;
break;
case 0x587:
BatteryStatusCharge_rcv(RxFrame, &rx_BSC); //Receive frame
BatteryStatusCharge_memHandler(rx_BSC, h_BSC); //handle memory
BSCFlag++;
break;
case 0x580:
BatteryStatusGeneral_rcv(RxFrame, &rx_BSG); //Receive frame
BatteryStatusGeneral_memHandler(rx_BSG, h_BSG); //handle memory
BSGFlag++;
break;
case 0x59f:
BatteryVehicleHandling_rcv(RxFrame, &rx_BVH); //Receive frame
BatteryVehicleHandling_memHandler(rx_BVH, h_BVH); //handle memory
BVHFlag++;
break;
case 0x24:
EPIC_PMZ_A_rcv(RxFrame, &rx_pmzA); //Receive frame
EPIC_PMZ_A_memHandler(rx_pmzA, h_PMZ_A); //handle memory
break;
case 0x50:
EPIC_PMZ_C_rcv(RxFrame, &rx_pmzC); //Receive frame
EPIC_PMZ_C_memHandler(rx_pmzC, h_PMZ_C); //handle memory
break;
case 0x5A:
EPIC_PMZ_E_rcv(RxFrame, &rx_pmzE); //Receive frame
EPIC_PMZ_E_memHandler(rx_pmzE, h_PMZ_E); //handle memory
break;
case 0x5E:
EPIC_PMZ_G_rcv(RxFrame, &rx_pmzG); //Receive frame
EPIC_PMZ_G_memHandler(rx_pmzG, h_PMZ_G); //handle memory
break;
case 0x60:
EPIC_PMZ_H_rcv(RxFrame, &rx_pmzH); //Receive frame
EPIC_PMZ_H_memHandler(rx_pmzH, h_PMZ_H); //handle memory
break;
case 0x4e2:
EPIC_PMZ_I_rcv(RxFrame, &rx_pmzI); //Receive frame
EPIC_PMZ_I_memHandler(rx_pmzI, &h_PMZ_I); //handle memory
break;
case 0x621:
HMI_DATA1_rcv(RxFrame, &rx_cluster); //Receive frame
HMI_DATA1_memHandler(rx_cluster, h_HMI); //handle memory
break;
case 0x719:
UDS_DIAG_rcv(RxFrame);
UDSFlag ++;
break;
case 0x700:
DCDC700_rcv(RxFrame, &rx_dcdc700); //Receive frame
DCDC700_memHandler(rx_dcdc700, DCDC_700); //handle memory
break;
case 0x703:
DCDC703_rcv(RxFrame, &rx_dcdc703); //Receive frame
break;
default:
sprintf(msg, "Unknown ID in FIFO 1\r\n");
HAL_UART_Transmit(&huart2, (uint8_t*)msg, strlen(msg), HAL_MAX_DELAY);
break;
}
}
}imultaneously. Then i used only one to receive the frames and it works.
2024-05-16 1:13 AM - edited 2024-05-16 1:15 AM
Hello,
Try first with "passing all messages" filter to be sure it's not a filter config issue:
canfilterconfig.FilterIdHigh = 0,
canfilterconfig.FilterIdLow = 0;
canfilterconfig.FilterMaskIdHigh = 0;
canfilterconfig.FilterMaskIdLow = 0;
PS: next time please use <\> button to insert your code. Thank you for your understanding.
2024-05-16 2:12 AM
Hello thank you for your quick answer.
I did what you said put 0 to cancel the filter. but nothing changed, here is a code of the following files: main.c; CanfilterConfig.c
main
void HAL_CAN_RxFifo0MsgPendingCallback(CAN_HandleTypeDef *hcan)
{
HAL_CAN_GetRxMessage(&hcan1, CAN_RX_FIFO0, &RxHeader, RxFrame);
{
switch(RxHeader.StdId)
{
case 0x586:
BatteryChargeCurrent_rcv(RxFrame, &rx_BCC); //Receive frame
BatteryChargeCurrent_memHandler(rx_BCC, &h_BCC); //handle memory
BCCFlag++;
break;
case 0x591:
BatteryCurrentLimit_rcv(RxFrame, &rx_BCL); //Receive frame
BatteryCurrentLimit_memHandler(rx_BCL, h_BCL); //handle memory
BCLFlag++;
break;
case 0x587:
BatteryStatusCharge_rcv(RxFrame, &rx_BSC); //Receive frame
BatteryStatusCharge_memHandler(rx_BSC, h_BSC); //handle memory
BSCFlag++;
break;
case 0x580:
BatteryStatusGeneral_rcv(RxFrame, &rx_BSG); //Receive frame
BatteryStatusGeneral_memHandler(rx_BSG, h_BSG); //handle memory
BSGFlag++;
break;
case 0x59f:
BatteryVehicleHandling_rcv(RxFrame, &rx_BVH); //Receive frame
BatteryVehicleHandling_memHandler(rx_BVH, h_BVH); //handle memory
BVHFlag++;
break;
default:
sprintf(msg, "Unknown ID in FIFO 0\r\n");
HAL_UART_Transmit(&huart2, (uint8_t*)msg, strlen(msg), HAL_MAX_DELAY);
break;
}
}
}
int main(void)
{
/* USER CODE BEGIN 1 */
/* USER CODE END 1 */
/* MCU Configuration--------------------------------------------------------*/
/* Reset of all peripherals, Initializes the Flash interface and the Systick. */
HAL_Init();
/* USER CODE BEGIN Init */
DID_Init();
/* USER CODE END Init */
/* Configure the system clock */
SystemClock_Config();
/* USER CODE BEGIN SysInit */
/* USER CODE END SysInit */
/* Initialize all configured peripherals */
MX_GPIO_Init();
MX_DMA_Init();
MX_USART2_UART_Init();
MX_CAN1_Init();
MX_ADC1_Init();
MX_TIM6_Init();
/* USER CODE BEGIN 2 */
CAN_Filter_FIFO0(&hcan1); // Filter config for FIFO0
CAN_Filter_FIFO1(&hcan1); // Filter config for FIFO1
HAL_CAN_Start(&hcan1);
HAL_CAN_ActivateNotification(&hcan1, CAN_IT_RX_FIFO0_MSG_PENDING); // Enable Interrupt at FIFO0 reception
HAL_CAN_ActivateNotification(&hcan1, CAN_IT_RX_FIFO1_MSG_PENDING); // Enable Interrupt at FIFO1 reception
HAL_TIM_Base_Start_IT(&htim6); // Start timer for scheduled frame sending
//HAL_ADC_Start_IT(&hadc1); // Start adc
/* USER CODE END 2 */
/* Infinite loop */
/* USER CODE BEGIN WHILE */
uint8_t countpres;
while (1)
{
/* USER CODE END WHILE */
/* USER CODE BEGIN 3 */
// if (uADCConversionCpltFlag) {
// uiADCRawValueBuffer = HAL_ADC_GetValue(&hadc1);
// sprintf(msg, "Throttle: %hu \r\n", uiADCRawValueBuffer);
// HAL_UART_Transmit(&huart2, (uint8_t *)msg, strlen(msg), HAL_MAX_DELAY);
// }
/*Single channel polling*/
// HAL_ADC_Start(&hadc1);
// HAL_ADC_PollForConversion(&hadc1, HAL_MAX_DELAY);
// uiADCRawValueBuffer = HAL_ADC_GetValue(&hadc1);
// sprintf(msg, "Throttle: %hu \r\n", uiADCRawValueBuffer);
// HAL_UART_Transmit(&huart2, (uint8_t *)msg, strlen(msg), HAL_MAX_DELAY);
/****************** USABLE CODE ******************/
/*SEND UDS RESPONSE*/
if(UDSFlag!=0)
{
UDSFlag = 0;
UDS_Response_mgt(RxFrame, VCU_Response, &TxHeader, TxFrame);
CAN_Send_Periodic();
}
if(BCCFlag!=0)
{
BCCFlag = 0;
Discharge_Battery();
Discharge_DCDC();
sprintf(msg, "BatteryChargeCurrent frame received\r\n");
HAL_UART_Transmit(&huart2, (uint8_t*)msg, strlen(msg), HAL_MAX_DELAY);
}
if(BCLFlag!=0)
{
BCLFlag = 0;
Discharge_Battery();
Discharge_DCDC();
sprintf(msg, "BatteryCurrentLimit frame received\r\n");
HAL_UART_Transmit(&huart2, (uint8_t*)msg, strlen(msg), HAL_MAX_DELAY);
}
if(BSCFlag!=0)
{
BSCFlag = 0;
Discharge_Battery();
Discharge_DCDC();
sprintf(msg, "BatteryStatusCharge frame received\r\n");
HAL_UART_Transmit(&huart2, (uint8_t*)msg, strlen(msg), HAL_MAX_DELAY);
}
if(BSGFlag!=0)
{
BSGFlag = 0;
Discharge_Battery();
Discharge_DCDC();
sprintf(msg, "BatteryStatusGeneral frame received\r\n");
HAL_UART_Transmit(&huart2, (uint8_t*)msg, strlen(msg), HAL_MAX_DELAY);
}
}
}
CanFilterConfig
#include "CanFilterConfig.h"
void CAN_Filter_FIFO0(CAN_HandleTypeDef* hcan)
{
CAN_FilterTypeDef canfilterconfig;
canfilterconfig.FilterActivation = CAN_FILTER_ENABLE;
canfilterconfig.FilterBank = 10;
canfilterconfig.FilterFIFOAssignment = CAN_FILTER_FIFO0;
canfilterconfig.FilterIdHigh = 0x580 << 5; // According to the DBC
canfilterconfig.FilterIdLow = 0x0000;
canfilterconfig.FilterMaskIdHigh = 0xfe0 << 5;// Calculation of the mask according to the DBC
canfilterconfig.FilterMaskIdLow = 0x0000;
canfilterconfig.FilterMode = CAN_FILTERMODE_IDMASK;
canfilterconfig.FilterScale = CAN_FILTERSCALE_32BIT;
canfilterconfig.SlaveStartFilterBank = 13;
HAL_CAN_ConfigFilter(hcan, &canfilterconfig);
}
Thank you again for your time
2024-05-16 2:16 AM
Hello,
Better to attach your main.c and your ioc files.
+ keep the filters to 0 for the moment.
2024-05-16 2:19 AM
2024-05-16 2:26 AM
Hello,
Thanks for the sharing,
Do you confirm you did a test with:
canfilterconfig.FilterIdHigh = 0,
canfilterconfig.FilterIdLow = 0;
canfilterconfig.FilterMaskIdHigh = 0;
canfilterconfig.FilterMaskIdLow = 0;
and didn't work?
2024-05-16 2:38 AM
Yes, i confirm that it is not working even with every fields set to 0.
2024-05-16 2:49 AM
Ok thank you.
Here I'm just pointing this statement:
"even though i can communicate with laptop for UDS protocole (Reception works properly in that case), but when i try with the battery, the debug mode doesn't stop at the rx interrupt routine."
So as I understand here, the receiving is working well when you send frames from your laptop (with a CAN bridge I suppose) but you couldn't receive any frame from the battery right?
2024-05-16 4:41 AM
Yes, actuallty i tried to communicate with BMS (directly on battery) but debug mode is not possible in that case so i am using the laptop to simulate the behavior but sending the frames i want, to test my state machine.
2024-05-16 6:35 AM
Anyways i just noticed that the frame is sent continuously from the laptop maybe it is the source of the problem. Gonna fix it, thank you very much for your support!
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.