2017-04-05 11:02 PM
Hello~all
I�m currently involved in a project and I am confusing about what chip can satisfy its need,please help me to chose economic one from STM32.I would like to chose STM32F103ZC,this is
STM32F103ZC�s
http://www.kynix.com/uploadfiles/pdf8798/STM32F103ZCT6.pdf
.Please help me have a look.The following states is the need of my project:
.the port:
1x RJ45 (TCP/IP)
,W5500 (I just know I need to use this one ,If you have a better one to recommend,please don�t hesitate to tell me.Thank you)
1x RS232,
1x RS485
1x SPI
1x I2C
6x 4-20ma
analogue input
R
elay--2*220V 10A is controlled by IO
Tube level output
of 30 mos are controlled by IO
T
wo pt100
4 digital temperature input of DS18B20
----end
Your help will be appreciated!
#stm322017-04-06 1:02 AM
It depends upon, what additional hardware onboard is available/planned to be used. For instance, you can use DS2484 - an I2C-to-1WIRE interface, - to talk to DS18B20. This would simplify the firmware and save CPU pins because only one I2C would be neccessary. To control 30 MOSFETs you can install some shift registers controlled over SPI or I2C expanders thus saving further pins, etc...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.