2013-07-31 1:17 PM
Hello,
I don't know if my understanding of NVIC is correct especially to System Tick Timer. &sharpinclude ''stm32f10x.h'' void NVIC_Configuration(void) { uint32_t priorityGroup; /* Variables to store priority group and priority */ uint32_t priority; NVIC_SetPriorityGrouping(1); /* 1 bits for pre-emption priority, 3 bits for subpriority */ priorityGroup = NVIC_GetPriorityGrouping(); /* Get used priority grouping */ priority = NVIC_EncodePriority(priorityGroup, 1, 3); /* Encode priority with 3 for subpriority and 1 for preempt priority */ NVIC_SetPriority(ADC1_2_IRQn, priority); /* Set new ADC1_2_IRQn priority */ NVIC_EnableIRQ(ADC1_2_IRQn); /* Enable ADC Interrupt */ priority = NVIC_EncodePriority(priorityGroup, 1, 1); /* Encode priority with 1 for subpriority and 1 for preempt priority */ NVIC_SetPriority(TIM1_CC_IRQn, priority); /* Set new TIM1_CC_IRQn priority */ NVIC_EnableIRQ(TIM1_CC_IRQn); /* Enable Timer1 CC4 Interrupt */ priority = NVIC_EncodePriority(priorityGroup, 1, 2); /* Encode priority with 2 for subpriority and 1 for preempt priority */ NVIC_SetPriority(TIM2_IRQn, priority); /* Set new TIM2_IRQn priority */ NVIC_EnableIRQ(TIM2_IRQn); /* Enable Timer1 CC4 Interrupt */ /* TIM4_IRQn should preempt all other interrupt (Highest Priority)*/ priority = NVIC_EncodePriority(priorityGroup, 0, 0); /* Encode priority with 0 for subpriority and 0 for preempt priority */ NVIC_SetPriority(TIM4_IRQn, priority); /* Set new TIM4_IRQn priority */ NVIC_EnableIRQ(TIM4_IRQn); /* Enable Timer1 CC4 Interrupt */ //NB: My main code does not work if I include the below section and Systick_Configuration(void) in main //Systick interrupt does nothing in my main code. Adding or Removing Systick interrupt supposed not to affect it //functionality.I just wanted to test my understanding of NVIC /* SysTick_IRQn lowest Priority */ priority = NVIC_EncodePriority(priorityGroup, 1, 6); /* Encode priority with 6 for subpriority and 1 for preempt priority */ NVIC_SetPriority(SysTick_IRQn, priority); /* Set new SysTick_IRQn priority */ NVIC_EnableIRQ(SysTick_IRQn); /* Enable SysTick_IRQn Interrupt */ } void Systick_Configuration(void) { if (SysTick_Config(SystemCoreClock / 1000)) //2KHz { /* Capture error */ while (1); } } void SysTick_Handler(void) { GPIOB->ODR ^= (1 << 8); } int main(void) { Systick_Configuration(); NVIC_Configuration(); RCC_Configuration(); //Configure System Peripherals Clock GPIO_Configuration(); //Configure Input & Output Pins ADC1_2_Configuration(); //Configure ADC1_2 in Dual Simultanous Sampling on a Single Channel PWM_Configuration(); //Configure Timer1 for 25KHz Independent Complementary PWM TIM4_Configuration(); TIM3_Configuration(); //Configure & Start Timer3 for Alignment and StartUp Phase TIM2_Configuration(); StartMotor(); //Start Motor while(1) { //Configure USART to Send and Receive Important Motor Details } } #nvic #stm322013-07-31 2:35 PM
Mostly, but you can't enable it as an ''IRQ'' because it's technically a system handler.
NVIC_EnableIRQ(SysTick_IRQn); // CAN'T DO THIS2013-07-31 3:57 PM
Hello,
Thanks..My code is functioning with SysTick_IRQn enable. Your correction was right.I shouldn't have re-enable SysTick_IRQn. RegardsWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.