2016-10-19 1:42 AM
Hello, I'm very new to STM32. I'm trying to generate some complex signal using internal DAC, using array of values. I would like to store this array in ROM (FLASH), since I need RAM for another task. Is it possible to transfer data from FLASH to DAC using DMA? Datasheet say: ''Access to Flash, SRAM, APB and AHB peripherals as source and destination'', but in STM32CubeMX I don't see FLASH option as data source...
#stm32 #dma #dac2016-10-19 2:21 AM
Which STM32 model?
Have you consulted the DMA section of the relevant RM? JWWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.