2020-05-13 5:27 AM
Is it possible to flash STM32 Nucleo board then power it with a battery and use it in an application without connecting it to PC?
2020-05-13 5:41 AM
Sure. The board doesn't care what is powering it. Probably needs to be connected to a PC to flash it.
2020-05-13 5:45 AM
Yes but i flashed a small program of blinking the green led of the Nucleo via ST link Utility! but nothing happened ! i can't see the led blinking, however i can see blinking with debug mode (via STM32CubeIDE) !
2020-05-13 6:13 AM
How exactly are you powering the board? There are guidelines in the user manual for valid power configurations. The ST-Link chip could be holding the other one in reset if not done correctly.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.