2014-03-05 1:29 AM
Hi,
I can't use the same timer in IAP code and user application code in the same time, even if I reset all registers and interrupts concerning this timer before jump to user application address. Note that I reallocated the vector table for the user application...Thank you2014-03-05 6:08 AM
Hi
''I can't use the same timer in IAP code and user application code in the same time'' When you say IAP - In Application Programming. Do you mean that you have written your own bootloader? ''I reset all registers and interrupts concerning this timer before jump to user application '' In general - it is a good idea to disable and re-configure all peripherals to be used in each application during startup. In the case of the timer - the timer must be disabled first before some of its registers can be changed (or the change take effect).2014-03-05 6:58 AM
Ok, should we guess what part you're using, and the code you constructed that is failing?
2014-03-05 10:24 PM
Hi again,
Thank you for your replies,Yes it's my own bootloader. I am using STM32F105, and this is the way I reset all timer registers and the USB peripheral before jumping to the main application...if (((*(__IO uint32_t*)ApplicationAddress) & 0x2FFE0000 ) == 0x20000000){ /* Reset all registers used in System file */ NVIC_DisableIRQ(TIM3_IRQn); RCC->APB1ENR &=~RCC_APB1ENR_TIM3EN; TIM3->CR1 = 0; // reset command register 1 TIM3->CR2 = 0; // reset command register 2 TIM3->PSC = 0; TIM3->ARR = 0; TIM3->DIER =0; // disable interrupt TIM3->CNT=0; TIM3->SR=0; /* Disable the USB clock */ RCC_APB1PeriphClockCmd((uint32_t)0x00800000, DISABLE); OTGD_FS_Handle_UsbReset_ISR(); PowerOff(); /* Jump to user application */ JumpAddress = *(__IO uint32_t*) (ApplicationAddress + 4); Jump_To_Application = (pFunction) JumpAddress; /* Initialize user application's Stack Pointer */ __set_MSP(*(__IO uint32_t*) ApplicationAddress); Jump_To_Application(); }Note the USB causes the same problem, it seems it still working and when I plug in a USB cable, the main application crushes and after 3 resets the bootloader works again automatically ...thank you2014-03-05 10:40 PM
You might want to try programming the TIM3 registers BEFORE disabling the clock to the peripheral, as the writes definitely won't work after the clock is stopped.
2014-03-05 11:25 PM
Thank you cliv1, you are right about Timer3... can you help me about how to disable correctly the USB??
2014-03-06 1:32 AM
Hi
I found the USB stack from the USB OTG does re-initialise OK. The issue is to do with disconnection - you will need to force a software disconnect. Depending on your processor, something like // force a USB soft disconnect // USB_OTG_dev.regs.DREGS->DCTL |= 0x02;2014-03-06 1:52 AM
Thank you sung.chen_chung, that is what I did and it solved my problem ...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.