2016-10-20 7:34 PM
Is possible to interface two STM32's one F7 and one F4 via the Flexible Memory Controller?
Thanks for the help. #stm32f4 #fmc #fmsc2016-10-21 12:03 PM
You can use dual port sram to interface 2 STM32 to each other. Split the memory into two areas software wise with RO / WO for each uC and you are done. But be aware that dual port sram is expensive and often used in FPGA systems to interface the FPGA to an uC.
2016-10-21 12:20 PM
FIFO type buffering?
http://www.averlogic.com/AL422B.asp
You might be able to use FSMC to DCMI, or a GPIO/DMA arrangementCan't go directly FSMC-to-FSMC as there is no good way of initiating a transfer on the receiving end, hence the DualRAM suggestion, or an FPGA mitigating interaction, and IRQ's etc.2016-10-22 2:53 PM
Thanks for the answer.
I was trying to avoid Dual Port RAM for a cheap prototype, I think I'll try Quad-SPI betterWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.