2013-08-03 4:12 AM
2015-06-02 1:58 AM
Even in HAL drivers is written:
(+) Exit:(++) By issuing an interrupt or a wakeup event, the MSI RC oscillator is selected as system clock.
It's not true, because even IWDG will make a reset in this mode which is so bad and can't be avoided in any way.
2016-12-15 1:21 PM
No, it can be avoided. Per the STM manuals there is something called the IWDG_STOP bit in the FLASH_OPTR register, which (if set) freezes the IWDG during stop. I'm actually digging through the forum looking for more explanation of what this means!
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.