2023-02-23 2:34 AM
I am using STM32F401CCU6 for making Oscilloscope with Waveform on display, I need to display upto 1kHz waveform in 300points. For that i am using 4Channels ADC with DMA and timer for Triggering.
The code used for ADC starting :
if(HAL_OK != HAL_ADC_Start_DMA(&hadc1,(uint32_t *)adcRead, bufferSize * ChannelCount)){
Error_Handler();
}where adcRead is Main DMA buffer ,
bufferSize is Buffer Size for 1 channel,
channelCount is No. of Channels (in my case 4 channels)
after One DMA transfer , I use ADC callback function to stop ADC :
void HAL_ADC_ConvCpltCallback(ADC_HandleTypeDef* hadc){
if(HAL_ADC_Stop_DMA(&hadc1) != HAL_OK){
errorcount++;
Error_Handler();
}
}After displaying one Buffer , I start ADC again using above starting code again.
To seperate each channel data from Main buffer , I used
for (int i = 0; i < bufferSize; i++) Adc0[i] = adcRead[(i*ChannelCount) + 0];
for (int i = 0; i < bufferSize; i++) Adc1[i] = adcRead[(i*ChannelCount) + 1];
for (int i = 0; i < bufferSize; i++) Adc2[i] = adcRead[(i*ChannelCount) + 2];
for (int i = 0; i < bufferSize; i++) Adc3[i] = adcRead[(i*ChannelCount) + 3];BUT the main problem arising here is that,
data of different channel interchanges randomly.
sometime channel 1 waveform in channel 2 or 3 or 4
and vice versa.
I am using max ADC clock , that is 36mHz.
I can't find the problem.
Thank You.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.