2020-10-24 8:14 AM
IN NUCLEO-144H743 , only 3 ADC channels IN3 ,IN18 ,IN19 working in ADC 1
If I use INP5 or INP6, I am not reading anything,
I am using Example ADC_RegularConversion_Polling replacing sConfig.Channel with ADC_CHANNEL_5 and 6;
Am I missing any Configuration?
2020-10-24 9:02 AM
> If I use INP5 or INP6, I am not reading anything,
What does this mean? Presumably there is a value making it to the ADCx->DR register. Is it incorrect? Too high, low?
> Am I missing any Configuration?
Maybe. You haven't given us much to work with. You'll need to initialize all ADC pins in use in analog mode.
2020-10-25 4:24 AM
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.