2020-07-15 1:26 PM
Hello,
We are using the STM32H745 dual core series, and have an image size that is nearing the single flash banks limit of 1MB. We won't be using the swap bank feature at any point. Will there be issues if the image overlaps the second bank?
2020-07-15 1:30 PM
Also, let's assume the default boot address of the 2nd core (M4) is moved further down the flash address space
2020-07-15 1:31 PM
> Will there be issues if the image overlaps the second bank?
Nope. The banks are contiguous so just define it as a single block of size 2MB and it'll work.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.