2015-10-22 1:07 AM
Is there any working example for IKS01A1 sensor board and STM32F103 nucleo board? I couldn't find any in offical examples.
#x-nucleo-iks01a1 #nucleo-stm32f2015-10-22 8:25 AM
Hi cctt,
X-NUCLEO-IKS01A1 has a X-CUBE-MEMS1 software package that contains examples, but it is compatible only with NUCLEO-F401RE, NUCLEO-L053R8 or NUCLEO-L152RE. For more informations, visit this .-Shahrzad-2017-01-27 11:57 PM
I am sure you have managed to use F103.
In my case (wanted to use F411 with the MEMs sensor board) I simply:
-opened the example for F401 (the one with Terminal Logging) in Keil
-replaced the F401 device with F411 in Options->Device tab
-In Options->C/C++ tab enter the 'USE_HAL_DRIVER,STM32F411xE,USE_STM32F4XX_NUCLEO,VECT_TAB_SRAM, RAM_MODE, REMAP' - notice the only change is the F411-related item
I wonder if there is other way of doing it - perfectly how to add BSP to CubeMX generated project, not as in my case stupid changes in original project.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.