2018-05-03 4:55 AM
Hi
When I press the button Vo is not = vin, no respond to the button at all.Any suggestions ?#include <LiquidCrystal.h>LiquidCrystal lcd(PA0, PA1, PA2, PA3, PA4, PA5);int analogInput = PB0;const int ResetPin = PA7;float vout = 0.0;float vin = 0.0;float Vo;int value = 0;
void setup() {// pinMode(PB0,analogInput, INPUT);
pinMode(PB0, INPUT_ANALOG); pinMode(ResetPin, INPUT); Vo = analogRead(INPUT_ANALOG); lcd.begin(16, 2); //lcd.print('DC V');}void loop() {if (digitalRead(ResetPin) == LOW) { Vo = vin; } else { // read the value at analog input value = analogRead(analogInput); vout = (value * 3.3) / 4200.0; vin = vout; if (vin < 0.09) vin = 0.0; //statement to quash undesired reading ! } lcd.setCursor(0, 1); lcd.print('V= '); lcd.print(vin); lcd.setCursor(0, 0); lcd.print('Vo= '); lcd.print( Vo, 1); delay(500);}We’re moving the ST Community to a new platform to give you a better and more reliable community experience.