2015-11-20 2:22 AM
1. Timer Configuration
Add the
timer
configuration
calculator
which of
the requested Interupt Time or Frequency calculate Counter Period (ARR) and
conversely
the
input values
shows the parameters
counter.
Excellent
would be
a graphical
display of output
PWM
etc.
2. Timer ConfigurationNow
we see Clock Source: Internal clock
Why
not see
currently set
value of Internal Clock?
3.Graphical
highlighting
functional groups
of pins
For example, When scroll overUART
inlist
Pinout t
hey might
highlight
pins
occupied
this Peripheral .
If the
periphery of
the conflict
highlight
graphically
what
pin.
This is important
especially
if you
are using
STM32Cube
simultaneously
with the
hardware (PCB) design.
2015-11-20 6:40 AM
Hi Charles,
Thanks for the suggestion! I will forward this to our team.-Syrine –2015-11-27 4:42 AM
Hi Charles
Could you be more precise on your request ''1. timer configuration'' : - What do you want to use the timer for ? - What will be the ''inputs'' and the ''outputs'' of what you call ''timer configuration calculator'' : I didn't catch, for example, if you imagine the ''PWM output waveform'' as an Input or an Output. Concerning ''2. Timer Configuration'' : - Where do you except to see the ''Internal clock'' value ? Directly in the ''Pinout view'', when selecting ''Clock Source'' (as Internal Clock or ETR2 or ETR2...) regards,We’re moving the ST Community to a new platform to give you a better and more reliable community experience.