2013-06-06 10:08 AM
I'm a beginer with IAR.
I selected the st_link for the debugger but this error is generated :''Fatal error: ST-Link, Failed to identify target MCU - Check hardware and interface selected Session aborted! '' I tried one of the project that are included in IAR it work fine. so the problem is not from the driver.2013-06-06 10:19 AM
Do you have SWD mode selected? JTAG mode won't work.
Pay very careful attention to the settings in the project that works, and compare those with the one that fails.2013-06-06 10:22 AM
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.