2017-08-01 7:26 AM
Hi
I am new to using STM devices. I have bought this EVB STM32F407VGT6 MCU board. I would like to know where to download the IAR development tool for this... I am used to using the word IDE or CCS.. I would like to know the equivalent for this for STM.. Thanks.
2017-08-01 8:34 AM
I believe you'd want to go direct to IAR and purchase the tool or demos from there.
https://www.iar.com/iar-embedded-workbench/partners/stmicroelectronics/
IAR and Keil, are both IDE (Integrated Development Environment, it's an abbreviation)
ST's CubeMX can output code for either of those IDE, and others, and includes example code for ST's EVAL, DISCO and NUCLEO boards. Third-party board support would need to come primarily from the Third-Party selling the board.
2017-08-01 8:53 AM
Hello,
Hope these links helps you:
Best Regards
Imen
2017-08-01 10:30 AM
>>
I have bought this EVB STM32F407VGT6 MCU board.
This lacks specificity, this is a chip not a board, perhaps provide a cite of the specific make/model of board you're talking about. An STM32F407G-DISC1?
2017-08-01 12:45 PM
Hello
If you are interested in trying Keil: here are a couple of hands-on labs that might be useful considering which board you have: These are for STM32F407-DISCO:
2017-08-01 1:03 PM
Hi
I have installed the IAR embedded workbench IDE. Now if i want to use this IDE to run example code for STM MCUs... Where can I find some example code/project of STM MCU and especially the MCU STM32F407. Thanks.
2017-08-02 2:36 AM
Hi,
You have to download the
and you will find a full set of examples as:STM32Cube_FW_F4_V1.16.0\Projects\STM32F4-Discovery\Examples
Best Regards
Imen
2017-08-02 9:20 AM
What board specifically do you have? EVB is a bit generic and nonspecific.
The project examples under the Cube installation support several boards with the 407 chip onboard, say the STM3240G-EVAL or STM32F4-DISCO, the value of these will depend on if you need to port pins for peripherals, or LED, etc to match those of your board.
The examples broadly will cover an array of F4 parts, all extremely similar.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.