2007-12-20 9:58 AM
IAP Driver failed with an image more than 16K?
2011-05-17 3:20 AM
Hi,
I try to use the IAP driver(from AN2557) in my project. If the user code is less than 16K, it works well. But when loading a bigger binary file, the communications stopped after 15K bytes downloaded. And I only modified the IAP start condition from ''push button read'' to check a special value in backup register.2011-05-17 3:20 AM
Hi leiyuebit,
Do you have an error message ? or something else. You can try reducing the USART Baudrate if it has en effect or not. Thank you. Stone-32.We’re moving the ST Community to a new platform to give you a better and more reliable community experience.