2023-10-25 6:46 PM
I would like to use NUCLEO-H753ZI (STM32H753ZITxLQFP144) to do the following:
・Use ADC1 and ADC2 to start acquiring separate signals in a circular buffer at 1MSa/s. (The time of each ADC is synchronized.)
(1) Start ADC using the following function
Function name: HAL_ADCEx_MultiModeStart_DMA
(2) Once half of the data in the circular buffer has accumulated, acquire the ADC1 and ADC2 signals and execute any processing.
Function name: HAL_ADC_ConvHalfCpltCallback
How should I set it on STM32CubeMX?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.