2022-04-06 8:29 AM
2022-04-06 8:36 AM
SPI -> DMA -> SRAM -> ?
That way you will only get DMA (half-) complete interrupts, how often depends on your buffer size.
Depending on what you want to do with the ADC data, I'd recommend an STM32 with DMA supporting double buffering.
2022-04-06 8:56 AM
Hi, yes that is my intention. But my isues is i need to use the chip select for an input to the adc as a conversion start trigger. But when configureing the spi as a master format motorola and enable the NSS i need to enable and disable the spi to get NSS toggling.
/* Disable all peripherals for now*/
DMA2_Stream5->CR = 0;
DMA2_Stream2->CR = 0;
TIM1->CR1 = 0;
SPI1->CR1 = 0;
/* USER CODE END SysInit */
/* Initialize all configured peripherals */
MX_GPIO_Init();
MX_USART2_UART_Init();
MX_DMA_Init();
MX_SPI1_Init();
MX_TIM1_Init();
/* USER CODE BEGIN 2 */
/* DMA2 SPI1 receive */
/* Setting source & target pointer for rx */
LL_DMA_SetMemoryAddress(DMA2, LL_DMA_STREAM_2, (uint32_t)adc_data);
LL_DMA_SetPeriphAddress(DMA2, LL_DMA_STREAM_2, (uint32_t)&SPI1->DR);
LL_DMA_SetDataLength(DMA2, LL_DMA_STREAM_2, ADC_VALUE_COUNTS);
DMA2_Stream2->FCR = 0;
/* enable spi to do req on dma */
LL_SPI_EnableDMAReq_RX(SPI1);
/* DMA2 start now for rx*/
LL_DMA_EnableStream(DMA2, LL_DMA_STREAM_2);
/* start SPI now */
LL_SPI_Enable(SPI1);
/* Setting source & target pointer for tx */
LL_DMA_SetMemoryAddress(DMA2, LL_DMA_STREAM_5, (uint32_t)adc_channel);
LL_DMA_SetPeriphAddress(DMA2, LL_DMA_STREAM_5, (uint32_t)&SPI1->DR);
LL_DMA_SetDataLength(DMA2, LL_DMA_STREAM_5, ADC_CHANNEL_COUNTS);
DMA2_Stream5->FCR = 0;
temp = DMA2_Stream5->CR;
/* DMA2 start now for tx*/
LL_DMA_EnableStream(DMA2, LL_DMA_STREAM_5);
/* start TIM1 now and start update event*/
LL_TIM_EnableDMAReq_UPDATE(TIM1);
LL_TIM_EnableCounter(TIM1);well this runs in an endless loop but with no control of the chip select. How could i have control of the NSS pin without using interrupts, because other wise i could do all in the interrupt.
Greetings
2022-04-06 9:16 AM
Then it's probably not going to work ideally.
For these types of things people typically add glue logic, in the form of a state-machine, or other combinatorial logic, in a CPLD, or something, to smooth the disparity in expectations, and can do so at wire rates.
2022-04-06 2:10 PM
Which STM32?
> How could i have control of the NSS pin without using interrupts
Using timers.
One way to pull this off is to generate both the framing and SPI SCK from two master-slave-coupled timers, and feed it back externally to SPI set as slave.
Sometimes this sort of protocols can be pulled off quite easily using the SAI module.
JW
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.