2020-03-07 1:17 PM
2020-03-08 8:11 AM
Undo what you did to make it stop working.
2020-03-08 8:47 AM
I dont know what caused this, actually I have a guess. I touched the debugger and led turned off. So static might caused this. Any suggestion?
2020-03-08 9:05 AM
ESD can definitely kill things. If it's a ST board, and the computer can't recognize the debugger after a reset, I would guess it's dead. Although that would be uncommon. Does it show up as connected in the device manager? Does the board have the correct voltage level? Not sure if the LED is tied directly to power or not, but you could check that in the schematic to help diagnose.
2020-03-08 12:07 PM - edited 2023-11-20 9:32 AM
I have discovery board.
Device manager says unknown usb device (device identifier operation failed). On 5 V pin I measured 4.78 V and 3V pin 2.99 V.
Led that turned off is COM led.
2020-03-08 12:28 PM
2020-03-08 1:07 PM
So is there any way to fix it or it is dead?
2020-03-08 1:20 PM
2020-03-08 1:37 PM
Okay. Thanks.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.