2022-04-14 9:12 AM
Mantion some details
->in this STM32L475VG DISCOVRY KIT Rxfifo and Txfifo of spi is 32-bit
data register is 16-bit
->data register is send on Txfifo and receive from Rxfifo
2022-04-14 4:07 PM
Sounds like the master and slave are out of sync. You need to ensure the slave is ready to send when CS goes low, and that it's not stuck with stale data. You can re-enable the peripheral to clear the FIFO.
2022-04-14 6:03 PM
yes, i was try to complete process of Disable spi and re-enable after every one transaction but not solve.
spi SCL is control by Master so ,
1) in interrupt mode, working fine because after receiving data in Rxfifo(master) it start to read.
2) in polling mode, Master start clock and consider Rxfifo(master) is received data based on timing. its possible ?
so we get blank for first transaction.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.