2020-10-25 9:49 AM
Initially my board was working well with and without debugging mode, but when I changed microcontroller, it was working correctly in only debugging mode.
2020-10-25 10:09 AM
In debugging mode, I receive and send data correctly using usart1, but switch off the power and then power on(means reset the power) I am not getting all correct data on uart1, some of the character changed in a string, I also tried on uart 4, usart7 but facing same problem. Problem in only uart, other peripherals like ADCs, I2C, SPI working well.
Initially UART was also working well, but due to shorting between supply 3.3V and ground, microcontroller was damaged, I replaced a new one and getting problem in uart, all other peripherals are working well only problem in uart.
Anybody suggest its solution, what is the reason for this?
Thanks in advance.
2020-10-25 11:42 AM
For self designed boards look at BOOT0 pin state, should be pulled LOW.
Check Option Settings, with regard to boot address.
The wrong boot setting can result in code execution from ROM, not your own code.
Your code may also be executing, but stuck in a while() loop, often Error_Handler() or HardFault_Handler(), instrument these properly so you can determine if it is there.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.