2023-05-13 10:06 AM
2023-05-13 11:15 AM
The GPIO's that are 5v tolerant have clamping diodes which won't let the voltage go above VDD.
2023-05-14 7:17 AM
>>Can anyone explain it to me?
Probably relates to the dictionary definition of "tolerant", you should look that up.
Chances are that a 3.3V you're well into the VIN-HIGH threshold for 5V systems
You could try using the pin in Open-Drain, with an external pull-up to 5V
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.