2020-01-06 10:30 AM
I use Cube MX to configure pins and peripherals.
I think that is board issue but I can't find the reason.
Thanks
2020-01-06 11:53 AM
Running from ROM, make sure BOOT(0) pin is pulled LOW to run from FLASH, check option-bytes on chips without BOOT pins.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.