2022-11-16 6:14 AM
Hi ,
I am using STM32F051K6U7 for one of our project.
For Timing the HAL_GetTick() is low accuracy .
every 240 seconds there are 1 to 2 seconds off .
I am using a f0discovery board, so I am using internal RC occilator.
Is this expected or is there an errata to consider to fix it ?.
2022-11-16 8:38 AM
if you look in ds , see RC osz. about 1% , is about 2 s in 200 s, to expect. right ?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.