2020-03-23 10:30 AM
Please help me.
My code
SPI Master Code----------------------
Initialization
/* SPI4 init function */
void MX_SPI4_Init(void)
{
hspi4.Instance = SPI4;
hspi4.Init.Mode = SPI_MODE_MASTER;
hspi4.Init.Direction = SPI_DIRECTION_2LINES;
hspi4.Init.DataSize = SPI_DATASIZE_16BIT;
hspi4.Init.CLKPolarity = SPI_POLARITY_LOW;
hspi4.Init.CLKPhase = SPI_PHASE_2EDGE;
hspi4.Init.NSS = SPI_NSS_SOFT;
hspi4.Init.BaudRatePrescaler = SPI_BAUDRATEPRESCALER_8;
hspi4.Init.FirstBit = SPI_FIRSTBIT_MSB;
hspi4.Init.TIMode = SPI_TIMODE_DISABLE;
hspi4.Init.CRCCalculation = SPI_CRCCALCULATION_DISABLE;
hspi4.Init.CRCPolynomial = 7;
hspi4.Init.CRCLength = SPI_CRC_LENGTH_DATASIZE;
hspi4.Init.NSSPMode = SPI_NSS_PULSE_DISABLE;
if (HAL_SPI_Init(&hspi4) != HAL_OK)
{
Error_Handler();
}
}
void HAL_SPI_MspInit(SPI_HandleTypeDef* spiHandle)
{
GPIO_InitTypeDef GPIO_InitStruct = {0};
if(spiHandle->Instance==SPI4)
{
/* USER CODE BEGIN SPI4_MspInit 0 */
/* USER CODE END SPI4_MspInit 0 */
/* SPI4 clock enable */
__HAL_RCC_SPI4_CLK_ENABLE();
__HAL_RCC_GPIOE_CLK_ENABLE();
/**SPI4 GPIO Configuration
PE2 ------> SPI4_SCK
PE5 ------> SPI4_MISO
PE6 ------> SPI4_MOSI
*/
GPIO_InitStruct.Pin = GPIO_PIN_2|GPIO_PIN_5|GPIO_PIN_6;
GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;
GPIO_InitStruct.Pull = GPIO_NOPULL;
GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_HIGH;
GPIO_InitStruct.Alternate = GPIO_AF5_SPI4;
HAL_GPIO_Init(GPIOE, &GPIO_InitStruct);
/* USER CODE BEGIN SPI4_MspInit 1 */
/* USER CODE END SPI4_MspInit 1 */
}
}
Main code
while (1)
{
/* USER CODE END WHILE */
/* USER CODE BEGIN 3 */
HAL_Delay(4000);
spiDataTx[0]++;
HAL_GPIO_WritePin(GPIOF, GPIO_PIN_4, GPIO_PIN_RESET);
HAL_SPI_Transmit(&hspi4, (uint8_t *)spiDataTx, 1, HAL_MAX_DELAY);
while(HAL_SPI_GetState(&hspi4)!=HAL_SPI_STATE_READY){}
HAL_SPI_Receive(&hspi4, (uint8_t *)spiDataRx, 1, HAL_MAX_DELAY);
HAL_GPIO_WritePin(GPIOF, GPIO_PIN_4, GPIO_PIN_SET);
//HAL_SPI_FlushRxFifo(&hspi4);
}
/* USER CODE END 3 */
Slave code-----------------
Initialization
/* SPI2 init function */
void MX_SPI2_Init(void)
{
hspi2.Instance = SPI2;
hspi2.Init.Mode = SPI_MODE_SLAVE;
hspi2.Init.Direction = SPI_DIRECTION_2LINES;
hspi2.Init.DataSize = SPI_DATASIZE_16BIT;
hspi2.Init.CLKPolarity = SPI_POLARITY_LOW;
hspi2.Init.CLKPhase = SPI_PHASE_2EDGE;
hspi2.Init.NSS = SPI_NSS_HARD_INPUT;
hspi2.Init.FirstBit = SPI_FIRSTBIT_MSB;
hspi2.Init.TIMode = SPI_TIMODE_DISABLE;
hspi2.Init.CRCCalculation = SPI_CRCCALCULATION_DISABLE;
hspi2.Init.CRCPolynomial = 7;
hspi2.Init.CRCLength = SPI_CRC_LENGTH_DATASIZE;
hspi2.Init.NSSPMode = SPI_NSS_PULSE_DISABLE;
if (HAL_SPI_Init(&hspi2) != HAL_OK)
{
Error_Handler();
}
}
void HAL_SPI_MspInit(SPI_HandleTypeDef* spiHandle)
{
GPIO_InitTypeDef GPIO_InitStruct = {0};
if(spiHandle->Instance==SPI2)
{
/* USER CODE BEGIN SPI2_MspInit 0 */
/* USER CODE END SPI2_MspInit 0 */
/* SPI2 clock enable */
__HAL_RCC_SPI2_CLK_ENABLE();
__HAL_RCC_GPIOB_CLK_ENABLE();
/**SPI2 GPIO Configuration
PB12 ------> SPI2_NSS
PB13 ------> SPI2_SCK
PB14 ------> SPI2_MISO
PB15 ------> SPI2_MOSI
*/
GPIO_InitStruct.Pin = GPIO_PIN_12|GPIO_PIN_13|GPIO_PIN_14|GPIO_PIN_15;
GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;
GPIO_InitStruct.Pull = GPIO_NOPULL;
GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_HIGH;
GPIO_InitStruct.Alternate = GPIO_AF0_SPI2;
HAL_GPIO_Init(GPIOB, &GPIO_InitStruct);
/* SPI2 interrupt Init */
HAL_NVIC_SetPriority(SPI2_IRQn, 0, 0);
HAL_NVIC_EnableIRQ(SPI2_IRQn);
/* USER CODE BEGIN SPI2_MspInit 1 */
/* USER CODE END SPI2_MspInit 1 */
}
}
main code-------------------
/* Initialize all configured peripherals */
MX_GPIO_Init();
MX_SPI2_Init();
/* USER CODE BEGIN 2 */
HAL_SPI_Receive_IT(&hspi2, (uint8_t *)spiDataRx, 1);
/* USER CODE END 2 */
/* Infinite loop */
/* USER CODE BEGIN WHILE */
while (1)
{
if(spiRxStatus){
HAL_SPI_Transmit(&hspi2, (uint8_t *)spiDataRx, 1, HAL_MAX_DELAY);
HAL_SPI_Receive_IT(&hspi2, (uint8_t *)spiDataRx, 1);
spiRxStatus=0;
}
/* USER CODE END WHILE */
/* USER CODE BEGIN 3 */
}
SPI Rx callback-------------------
void HAL_SPI_RxCpltCallback(SPI_HandleTypeDef *hspi)
{
/* Prevent unused argument(s) compilation warning */
UNUSED(hspi);
spiRxStatus=1;
/* NOTE : This function should not be modified, when the callback is needed,
the HAL_SPI_RxCpltCallback should be implemented in the user file
*/
}
2020-03-23 10:38 AM
Consider adding more details to make your post useful and/or answerable.
2020-03-23 10:44 AM
The SPI clock rate is limited to the maximum for the SPI port on the STM32F0. Check the datasheet for the port you are using on the 'F0. If you increase the 'F7 clock rate you must prescale the SPI clock to match the maximum 'F0 rate.
Jack Peacock
2020-03-23 10:55 AM
generally speaking the max spi clock speed is typically the slave max speed, which itself is typically SYSCLK/4 = 12 MHz. Master is typically SYSCLK/2 so change the prescaler to generate 12 MHz or less on SPI.SCK pin
2020-03-23 10:37 PM
I have added my code in Question Please verify
2020-03-24 2:40 AM
Thanks For reply
I have tried one by one all prescaler in master device.
hspi4.Init.BaudRatePrescaler = SPI_BAUDRATEPRESCALER_128;
How can I configure SPI clock in slave device?
2020-03-24 2:42 AM
Thanks For reply
I have tried one by one all prescaler in master device.
hspi4.Init.BaudRatePrescaler = SPI_BAUDRATEPRESCALER_128;
even at lowest speed its not working.
2020-03-24 2:44 AM
I have added my code in Question Please verify
2020-03-24 2:45 AM
I have added my code in Question Please verify
2020-03-24 3:50 AM
What are exactly symptoms of "not working"?
In master, you may need to add delays after NSS pin setting low/before setting high.
JW
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.