2021-11-24 2:35 AM
2021-11-24 7:14 AM
Try a different USB cable. Try a different USB port. Reboot. Make sure you are using the ST-Link USB connector if that's what you want to connect to, or the user USB connector with an appropriate program loaded (or the bootloader) if that's what you want to connect to.
2021-12-02 6:24 AM
Hello @KShin.1 ,
Were you able to resolve the issue you described here?
Did you tried @TDK 's suggestion ? Does it work ? If yes, please mark his reply as Best answer (click on "Select as Best").
Imen
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.