2024-10-14 3:49 PM
Many engineers I know use HT7533 as power supply for STM32F105RBT6 in automotive boards. I looked up the specs, and found that HT7533 is only rated for 100mA. Is it too low for STM32F105RBT6? Is TI's TPS7B91 or TPS7B92 better in this case? Thank you.
2024-10-15 12:29 AM
First of all, a note: the STM32F105RBT6 are not approved for automotive applications, so they may only be used there for additional devices.
As for your question: the STM32F105RBT6 itself requires a maximum current of slightly less than 100mA. However, there are several things to consider:
I have only picked out a few things to consider. For better help, you would need to provide a few relevant details about your application, e.g.
Regards
/Peter
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.