2019-11-17 6:21 AM
Hi
I read ADC 1 channel using DMA transfer to buffer array with length is 8.
int16_t aData[8];
HAL_ADC_Start_DMA(&hadc1, (uint32_t*) aData, 8);I want to average data each 8 convertions. I plan to use DMA Interrupt with a counter, when counter reach 8, I calculate average value. But I can not find any example on ST site or google
Anyone help me?
Thanks
2019-11-19 1:19 AM
Hello @Ngô Nam ,
You need to precise the device you are using, then you can look to the examples provided in the relevant STM32Cube package depending on the selected STM32 product.
-Amel
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2019-11-19 1:59 AM
I don't use Cube/HAL.
> I plan to use DMA Interrupt with a counter,...
DMA will give you a TC interrupt (transmission complete) when a configured transfer has finished.
If you configure 8 items, you will get the TC interrupt as you want it. Just calculate the average over that buffer.
Not sure how this is modeled in Cuba/HAL. I usually implemented exactly this mechanism, but based on the "old" SPL.
2019-11-19 5:14 AM
I tried, but didn't find out, anyway thanks
2019-11-19 5:15 AM
DMA has a Global Interrupt, but I can not find out how to call correctly
2019-11-19 5:34 AM
Some example code for the F407, though based on SPL. I do not do Cube/HAL.
Not complete, but hopefully enough to get the point.
Configures two channels of ADC3 for a TIM triggered conversion, and a DMA transfer through DMA2 Stream0 channel2, for 256 values each.
At the end, the DMA_IT_TC is enabled (interrupt on Transfer Complete).
#define ELFR_CFFT_LENGTH 256
#define ELFR_CFFT_LENGTH 256
#define AIN_CHANNELS 2
...
/* NVIC DMA interrupt setup - priority is 1, below sampling clock int. priority */
NVIC_InitStructure.NVIC_IRQChannel = DMA2_Stream1_IRQn;
NVIC_InitStructure.NVIC_IRQChannelPreemptionPriority = 1;
NVIC_InitStructure.NVIC_IRQChannelCmd = ENABLE;
NVIC_Init (&NVIC_InitStructure);
...
/* DMA2 Stream0 channel2 configuration **************************************/
DMA_InitStructure.DMA_Channel = DMA_Channel_2;
DMA_InitStructure.DMA_PeripheralBaseAddr = (uint32_t) ADC3_DR_ADDRESS;
DMA_InitStructure.DMA_Memory0BaseAddr = (uint32_t) &AdcBuffer;
DMA_InitStructure.DMA_DIR = DMA_DIR_PeripheralToMemory;
DMA_InitStructure.DMA_BufferSize = ELFR_CFFT_LENGTH * AIN_CHANNELS;
DMA_InitStructure.DMA_PeripheralInc = DMA_PeripheralInc_Disable;
DMA_InitStructure.DMA_MemoryInc = DMA_MemoryInc_Enable;
DMA_InitStructure.DMA_PeripheralDataSize = DMA_PeripheralDataSize_HalfWord;
DMA_InitStructure.DMA_MemoryDataSize = DMA_MemoryDataSize_HalfWord;
DMA_InitStructure.DMA_Mode = DMA_Mode_Circular;
DMA_InitStructure.DMA_Priority = DMA_Priority_High;
DMA_InitStructure.DMA_FIFOMode = DMA_FIFOMode_Disable;
DMA_InitStructure.DMA_FIFOThreshold = DMA_FIFOThreshold_HalfFull;
DMA_InitStructure.DMA_MemoryBurst = DMA_MemoryBurst_Single;
DMA_InitStructure.DMA_PeripheralBurst = DMA_PeripheralBurst_Single;
DMA_Init (DMA2_Stream1, &DMA_InitStructure);
DMA_Cmd (DMA2_Stream1, ENABLE);
/* Configure ADC3 Channels 10 + 12 pin as analog input **********************/
GPIO_InitStructure.GPIO_Pin = GPIO_Pin_0 | GPIO_Pin_2;
GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AN;
GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL;
GPIO_Init (GPIOC, &GPIO_InitStructure);
/* ADC Common Init **********************************************************/
ADC_CommonInitStructure.ADC_Mode = ADC_Mode_Independent;
ADC_CommonInitStructure.ADC_Prescaler = ADC_Prescaler_Div2; // CLK = (APB2_CLK / 2)
ADC_CommonInitStructure.ADC_DMAAccessMode = ADC_DMAAccessMode_Disabled;
ADC_CommonInitStructure.ADC_TwoSamplingDelay = ADC_TwoSamplingDelay_10Cycles;
ADC_CommonInit (&ADC_CommonInitStructure);
/* ADC3 Init ****************************************************************/
ADC_InitStructure.ADC_Resolution = ADC_Resolution_12b;
ADC_InitStructure.ADC_DataAlign = ADC_DataAlign_Right;
ADC_InitStructure.ADC_ScanConvMode = ENABLE; // DISABLE;
ADC_InitStructure.ADC_ContinuousConvMode = DISABLE;
ADC_InitStructure.ADC_NbrOfConversion = AIN_CHANNELS;
ADC_InitStructure.ADC_ExternalTrigConvEdge = ADC_ExternalTrigConvEdge_Rising;
ADC_InitStructure.ADC_ExternalTrigConv = ADC_ExternalTrigConv_T3_TRGO;
ADC_Init (ADC3, &ADC_InitStructure);
/* ADC3 regular channel7 configuration *************************************/
ADC_RegularChannelConfig (ADC3, ADC_Channel_10, 1, ADC_SampleTime_112Cycles);
ADC_RegularChannelConfig (ADC3, ADC_Channel_12, 2, ADC_SampleTime_112Cycles);
ADC_DMARequestAfterLastTransferCmd (ADC3, ENABLE);
ADC_DMACmd (ADC3, ENABLE); /* Enable ADC3 DMA */
ADC_Cmd (ADC3, ENABLE); /* Enable ADC3 */
TIM_Cmd (TIM3, ENABLE); /* TIM3 enable counter, to trigger ADC */
DMA_ITConfig (DMA2_Stream1, DMA_IT_TC, ENABLE); /* interrupt notification when the buffer full */Associated handler was called DMA2_Stream0_IRQHandler () within the SPL for this MCU.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.