2023-05-09 1:08 PM
I am using a Nucleo-L476RG board and I am using USART2 for serial communication. I bought the sparkfun QR scanner module and it has a TX and RX pin. Can I simply connect the TX pin from the scanner to the RX pin (PA3) of USART2 and receive the data from the QR scanner?
2023-05-09 1:35 PM
https://www.sparkfun.com/products/18088
https://www.robotics.org.za/SPX-16441
These look to generate CMOS levels, so TX to STM32 UART-RX, appropriate baud rate / format
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.