2025-01-20 2:40 AM - edited 2025-01-20 5:18 AM
I would like to use the WKUP 6 (RTC_WUT_S) to wake up from Standby mode. I am already using WKUP 7 with a pin so I need the RTC to be in safe mode.
What would be the best way?
Solved! Go to Solution.
2025-01-21 1:11 AM
Hello @JAltu.1 ,
You can't add Trustzone to an existing non-Trustzone application. you will have to start a new project with Trustzone enabled in order to have the isolation and security features that it offers with the secure and non-secure projects.
Regards
2025-01-20 9:15 AM
Hello @JAltu.1 ,
I don't get you exact request what do you mean by saying "RTC to be in safe mode".
are you working with trustzone enabled?
if yes then working with RTC in a safe way should be done by setting WUTSEC bit in control register
When WUTSEC is set:
– RTC_WUTR register, plus WUTE, WUTIE and WUCKSEL control bits in the
RTC_CR, CWUTF in the RTC_SCR, WUTF in RTC_SR, and WUTMF in
RTC_SMISR can be read and written only in secure mode.
– WUTPRIV in the RTC_PRIVCFGR can be written only in secure mode
please refer to RM0456 section 63.3.4 RTC secure protection modes for more details.
Regards
2025-01-20 11:57 PM
Hi @STea ,
Trustzone is disabled. I have seen it can be enabled creating a new project.
But how can I do it in a existing project?
Regards
2025-01-21 1:11 AM
Hello @JAltu.1 ,
You can't add Trustzone to an existing non-Trustzone application. you will have to start a new project with Trustzone enabled in order to have the isolation and security features that it offers with the secure and non-secure projects.
Regards
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.