2021-07-29 12:02 AM
hello. I try to run usart1 in stm32F769I-disco. It is declared as : The serial interface USART1 is directly available as a virtual COM port of the PC, connected to the ST-LINK/V2-1 USB connector CN1. I added MX_USART1_UART_Init(HAL_UART_Init) and call HAL_UART_Transmit but it seems to not working. please advice. thanks.
2021-07-29 6:21 AM
Do you have the correct pins selected?
Does the VCP show up in the device manager?
Show your actual code used.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.