2020-10-20 7:01 AM
Hi
By changing linker script file of GPIO_Toggle code such that it points to RAM . And loaded the .hex and .bin ( specifying start program address as 0x20000000 ). The code looks like get stuck and never toggles LED. But when run in debug mode through cubeIDE . I see LED toggling. Can you please point out what and where i need to do changes to make code run in RAM other than in linker script Using stm32h7b3i-dk , cubIDE and cubeprogramer.
Solved! Go to Solution.
2020-10-21 3:31 AM
I could make it work by changing .ld with this
RAM (xrw) : ORIGIN = 0x24000000, LENGTH = 1024K
Now i can run for RAM without issue.
2020-10-20 8:47 AM
I also uncommented this line
#define VECT_TAB_SRAM in "system_stm32h7xx.c" file.
All works well with debugger but when i load .hex to RAM the code does not run.
2020-10-21 3:31 AM
I could make it work by changing .ld with this
RAM (xrw) : ORIGIN = 0x24000000, LENGTH = 1024K
Now i can run for RAM without issue.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.