2021-10-01 11:58 PM
working on STM32f103 want to hold time on power reset, not able to do it so,
used backup register to write the data,
HAL_RTCEx_BKUPRead(&hrtc, RTC_BKP_DR1);
HAL_RTCEx_BKUPWrite(&hrtc, RTC_BKP_DR1,0x32F2);
any suggestion would be great....
2021-11-04 2:31 AM
Welcome, @SM.15, to the community!
Are you sure the STM32F103C8T6 is a genuine device?
Are you sure VBAT is connected to a power source (battery, capacitor)?
Did you follow the recommendations of e.g. the project RTC_Calendar, which can be found in the local or online repository (Projects/STM3210E_EVAL/Examples/RTC)?
E.g. did you enable write access using HAL_PWR_EnableBkUpAccess()?
Regards
/Peter
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.