2025-08-19 10:01 PM
I am working with an STM32C092CCT6 (STM32C0 series) and I need help with reading and writing variables into Flash memory.
I want to store a few configuration values (like integers or structures) that should persist after reset or power cycle.
From what I understand, I need to erase a Flash page first and then program data at a specific address.
I am not sure about the correct sequence for the C0 series (unlocking Flash, erasing, programming, and locking again).
I would like to know the best practice for data alignment (word/halfword).
Should I use HAL functions like HAL_FLASH_Program() or is direct register access recommended for reliability?
If anyone has a working example code snippet or reference for reading/writing user variables into Flash on STM32C0, it would be really helpful.
Thanks in advance!
Solved! Go to Solution.
2025-08-20 3:15 AM
Hello @anuj18ap ,
Please find below the steps for Flash Memory Operations:
Unlock Flash Memory:
Before performing any operation, the Flash memory must be unlocked. Use the HAL_FLASH_Unlock() function.
Erase Flash Page:
Flash memory must be erased prior to writing new data. Use the HAL_FLASHEx_Erase() function to erase a specific Flash page.
Program Flash Memory:
Write data to Flash memory using the HAL_FLASH_Program() function
Lock Flash Memory:
After completing all operations, lock the Flash memory by calling HAL_FLASH_Lock() to prevent accidental writes.
For a practical implementation, you can refer to the example FLASH_EraseProgram provided in the STM32CubeFW for the C0 series.
Kind regards,
2025-08-20 3:15 AM
Hello @anuj18ap ,
Please find below the steps for Flash Memory Operations:
Unlock Flash Memory:
Before performing any operation, the Flash memory must be unlocked. Use the HAL_FLASH_Unlock() function.
Erase Flash Page:
Flash memory must be erased prior to writing new data. Use the HAL_FLASHEx_Erase() function to erase a specific Flash page.
Program Flash Memory:
Write data to Flash memory using the HAL_FLASH_Program() function
Lock Flash Memory:
After completing all operations, lock the Flash memory by calling HAL_FLASH_Lock() to prevent accidental writes.
For a practical implementation, you can refer to the example FLASH_EraseProgram provided in the STM32CubeFW for the C0 series.
Kind regards,
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.