2015-04-11 1:49 PM
Hi to all, I have developed my own ST iNemo based board, and I'm trying to program it with the Discovery board. The iNemo board is connected to the VCC pin of the discovery for the power supply while programming, and the other connections are related to the swd connection.
My board includes the resistors (10k) connected to the iNemo SWD links. Someone can suggest me why my ST-Link Util does not connect with this configuration and says me ''Can not connect to target!Please select ''Connect Under Reset'' mode from Target->Settings menu and try again.If you're trying to connect to a low frequency application , please select a lower SWD Frequency mode from Target->Settings menu.'' Thank you2015-04-11 4:55 PM
You need to walk through your design, and verify it's actually functional.
Make sure the analogue supply is present, and that NRST isn't clamped low. If you have USART connectivity, strap BOOT0 High, and test that you can talk to the System Loader.2015-04-12 1:40 AM
I have attached my schematic, using SWD connector linked to my Discovery board, and discovery linked to the pc through the USB connection, my boot0 pin has to be connected to gnd or left floating?
My NRST is not clamped down since there is a reset button connecting NRST to GND. Thank you ________________ Attachments : 1.pdf : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006HznU&d=%2Fa%2F0X0000000bS2%2FJoUPddVEf_lJ4sMqBS8CkKs6Tde9mA6h1rSeGaMkYzQ&asPdf=false2015-04-12 5:39 AM
Actually I was suggesting you use a scope or meter and verify that NRST isn't clamped low, ie held in reset by one of a number of drivers.
2015-04-12 6:35 AM
USART1 is PA9/PA10
Would suggest you place the module in System Loader mode (BOOT0=High), and then in a terminal application like RealTerm, and 9600 8E1, send an 0x7F byte, and confirm if you can see an 0x79 response. See also the Flash Loader Demonstrator application. If the module is not powering correctly the STM32 will be unreachable via JTAG/SWD or USART.We’re moving the ST Community to a new platform to give you a better and more reliable community experience.